mini-SAS Connections reverse?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mini-SAS Connections reverse?

ソリューションへジャンプ
4,626件の閲覧回数
harsh_mistry
Contributor I

Hi

In our custom board design with i.MX8DualXPlus / i.MX8QuadXPlus,

We are going to use external adaptor IMX-LVDS-HDMI(935358716598) for sending the video signal over to HDMI monitor. On schematic observation, we see that the connections for the 36 pin mini-SAS connector on the main cpu board (MEK MCIMX8QXP-CPU) and on the adaptor are reverse as shown in the image here:

mini-SAS.png

1. Is this connection intentionally done to compensate the connection reversal that happens in the mini-SAS cable as shown here:

mini-SAS cable.JPG

2. Our main question is if we select the right angle connector (Molex #75783-0140) for our custom board and cable (Molex #795762103), will this work with the same pin connections?

Your timely response will be highly appreciated.

Regards,

Harsh

0 件の賞賛
返信
1 解決策
4,524件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Harsh,

I don’t have specific data here for you to refer to, but according to my experience, for LVDS signals, the distance of 60cm is not long and there should be no problem.

Have a nice day!

B.R,

Weidong

元の投稿で解決策を見る

5 返答(返信)
4,524件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Harsh,

See below, please!

1. The signals on Mini SAS are customized and non-standard.

2. For your design, you need to refer to the signal definition method on EVK.

3. For the signal definition of the Right Angle connector, please see the picture below.

OLED connector:

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_5.png

Hope these pictures for connections are help to you!

Have a nice day!

B.R,

weidong

0 件の賞賛
返信
4,525件の閲覧回数
harsh_mistry
Contributor I

Thank you for the reply but looks like this is a bit different than what we are planning to use.

We will be using the LVDS To HDMI daughter board from NXP.

We only wish to change the vertical mini-SAS connector on the MEK (with connections shown before) to a right angle connector on our custom board (Molex #75783-0140) (similar to the daughter board) somewhat like this:

MINI-SAS-1.JPG

The pin connections and current connector part# on MEK are shown here:

mek_mini-SAS.JPG

So we still have the same question as posted earlier.

Regards,

0 件の賞賛
返信
4,524件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Dear Harsh,

Here is my understanding for the connection, for you reference :

pastedImage_1.png

Hope it is helpful to you!

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信
4,524件の閲覧回数
harsh_mistry
Contributor I

Thank you for the response.

One more thing we would like to ensure is the cable length.

We are going to use Molex#  795762103. It is 600mm in length.

Can this affect the LVDS signal integrity?

What kind of measures do we have to take to ensure proper video signal transmission?

Regards

0 件の賞賛
返信
4,525件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Harsh,

I don’t have specific data here for you to refer to, but according to my experience, for LVDS signals, the distance of 60cm is not long and there should be no problem.

Have a nice day!

B.R,

Weidong