migration from QualLite to Quad core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

migration from QualLite to Quad core

1,156件の閲覧回数
saida
Contributor II

HI

we have developed a hew board based I.MX6 DualLite and we want to upgrate to Quad core based processor

what are the precautions need to take ?

is both are pin to pin compatible ?

thanks and regards

Saida

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,041件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Saida S,

The i.MX6DualLite and the i.MX6Quad are pin-to-pin compatible, provided that some design decisions are followed. You can see Application Note 4397 (link below) for more details.

https://www.nxp.com/docs/en/application-note/AN4397.pdf

The hardware requirements are in section 4 of the application note. Its recommended to design with the possibility to migrate to a smaller pin-to-pin compatible processor if you are interested in doing so at some point. If your design is done for the i.MX6Q it’s possible that you will need to make some layout changes if you didn’t follow the guidelines listed on the application note.

I hope this helps!

Regards,

0 件の賞賛
返信

1,041件の閲覧回数
saida
Contributor II

thank you

i will come back to you once i done the changes for any queries

regards

saida

0 件の賞賛
返信