migration from QualLite to Quad core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

migration from QualLite to Quad core

1,169 Views
saida
Contributor II

HI

we have developed a hew board based I.MX6 DualLite and we want to upgrate to Quad core based processor

what are the precautions need to take ?

is both are pin to pin compatible ?

thanks and regards

Saida

Labels (2)
0 Kudos
Reply
2 Replies

1,054 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Saida S,

The i.MX6DualLite and the i.MX6Quad are pin-to-pin compatible, provided that some design decisions are followed. You can see Application Note 4397 (link below) for more details.

https://www.nxp.com/docs/en/application-note/AN4397.pdf

The hardware requirements are in section 4 of the application note. Its recommended to design with the possibility to migrate to a smaller pin-to-pin compatible processor if you are interested in doing so at some point. If your design is done for the i.MX6Q it’s possible that you will need to make some layout changes if you didn’t follow the guidelines listed on the application note.

I hope this helps!

Regards,

0 Kudos
Reply

1,054 Views
saida
Contributor II

thank you

i will come back to you once i done the changes for any queries

regards

saida

0 Kudos
Reply