microphone for MCIMXABASEV1(Baseboard)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

microphone for MCIMXABASEV1(Baseboard)

3,040 Views
abhirupmitra
Contributor II

Hi ,

I have MCIMXABASEV1 with imx6dl CPU card , I would like to know which microphone is suitable for the above mentioned baseboard.

Please share the suitable links.

Thanks in advance .

Abhirup Mitra

Labels (4)
Tags (2)
0 Kudos
Reply
5 Replies

2,922 Views
b36401
NXP Employee
NXP Employee

Unfortunately i.MX6 processors has no analog microphone input.
However it has SSI interface that supports I2S mode. So you can use to connect I2S microphone.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,922 Views
abhirupmitra
Contributor II

I agree with you Victor  but as I already mentioned , I have baseboard which has got microphone-in as well as audio-in & out ports.

I connected microphone in the RCA jacks, but am not able to record anything.IMG_20170519_110637.jpg

As you can see, we don't have a suitable microphone for the jacks which may be one reason for the problem.

Please give a solution for this!

Thanks ,

Abhirup

0 Kudos
Reply

2,922 Views
1015983812
Contributor I

What is the model number of the board that plugs in the microphone? Thank you!

0 Kudos
Reply

2,922 Views
b36401
NXP Employee
NXP Employee

Sorry, I did not noticed you already have the board, not designing it.

No. We have no special recommendation regarding to microphone for SABRE board.
Sorry for the inconvenience.

0 Kudos
Reply

2,922 Views
abhirupmitra
Contributor II

Thanks !

0 Kudos
Reply