mfgtool2: maximum size of file for UCL2 pipe command?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfgtool2: maximum size of file for UCL2 pipe command?

623件の閲覧回数
mikaelj
Contributor I

Hi,

I want to stream a 3GB file using the pipe command:

<CMD state="Updater" type="push" body="pipe dd of=/dev/mmcblk0 bs=1M" file="files/image.raw">Sending</CMD>

But file sizes >1GB will always fail, even though /dev/mmcblk0 is a 4GB eMMC. This on an MX6S.

Where is the limit documented? How do I lift the limit? I need to send this data to the device.

0 件の賞賛
返信
0 返答(返信)