mfgtool issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfgtool issue

2,937件の閲覧回数
victorien
Contributor IV

Hi,

I have a problem with mfgtool and an iMX28 on a custom board.

I generate updater_ivt.sb with ltib on ubuntu 12.04 and I use mfgtool 1.6.2.048 on windows 7 32bits.

The programming of the board works one time but now it doesn't work.

I have this log from mfgtool :

Friday, November 21, 2014 16:57:56

3 - Panel A Start processing SD Misu <LIST/>. 

Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="10" onError="" text="Booting hab update firmware.". 

3 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="10" onError="" text="Booting hab update firmware." SUCCESS code=0x0. 

Panel A Start <CMD/> type="find" body="Updater" file="" timeout="240" onError="" text="". 

Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE 

Panel A UtpUpdate Event: VolumeArrival Msg: (null) DevState: Updater OpState: WAITING_FOR_DEVICE 

3 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="240" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ echo Programmation" file="" timeout="10" onError="" text="DONE". 

3 - Panel A Finished <CMD/> type="push" body="$ echo Programmation" file="" timeout="10" onError="" text="DONE" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="mknod block,mmcblk0,/dev/mmcblk0,block" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="mknod block,mmcblk0,/dev/mmcblk0,block" file="" timeout="10" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="send" file="files/fdisk.input" timeout="10" onError="" text="Sending fdisk input". 

3 - Panel A Finished <CMD/> type="push" body="send" file="files/fdisk.input" timeout="10" onError="" text="Sending fdisk input" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ fdisk -u /dev/mmcblk0 < $FILE" file="" timeout="10" onError="" text="Partitioning SD card". 

3 - Panel A Finished <CMD/> type="push" body="$ fdisk -u /dev/mmcblk0 < $FILE" file="" timeout="10" onError="" text="Partitioning SD card" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p1,/dev/mmcblk0p1,block" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p1,/dev/mmcblk0p1,block" file="" timeout="10" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p2,/dev/mmcblk0p2,block" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p2,/dev/mmcblk0p2,block" file="" timeout="10" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p3,/dev/mmcblk0p3,block" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p3,/dev/mmcblk0p3,block" file="" timeout="10" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p5,/dev/mmcblk0p5,block" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p5,/dev/mmcblk0p5,block" file="" timeout="10" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p6,/dev/mmcblk0p6,block" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="mknod block/mmcblk0,mmcblk0p6,/dev/mmcblk0p6,block" file="" timeout="10" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ mkfs.vfat /dev/mmcblk0p3" file="" timeout="10" onError="" text="Formatting Linux partition". 

3 - Panel A Finished <CMD/> type="push" body="$ mkfs.vfat /dev/mmcblk0p3" file="" timeout="10" onError="" text="Formatting Linux partition" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ mkfs.ext3 /dev/mmcblk0p5" file="" timeout="10" onError="" text="Formatting rootfs partition". 

3 - Panel A Finished <CMD/> type="push" body="$ mkfs.ext3 /dev/mmcblk0p5" file="" timeout="10" onError="" text="Formatting rootfs partition" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ mkfs.vfat /dev/mmcblk0p6" file="" timeout="10" onError="" text="Formatting data partition". 

3 - Panel A Finished <CMD/> type="push" body="$ mkfs.vfat /dev/mmcblk0p6" file="" timeout="10" onError="" text="Formatting data partition" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ mkdir -p /mnt/mmcblk0p3" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="$ mkdir -p /mnt/mmcblk0p3" file="" timeout="10" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ mount /dev/mmcblk0p3 /mnt/mmcblk0p3" file="" timeout="10" onError="" text="". 

3 - Panel A Finished <CMD/> type="push" body="$ mount /dev/mmcblk0p3 /mnt/mmcblk0p3" file="" timeout="10" onError="" text="" FAIL code=0x2000. 

Panel A: Reason is unknown,failed to run command: type="push" body="$ mount /dev/mmcblk0p3 /mnt/mmcblk0p3" file="" timeout="10" onError="" text=""   

4 - Panel A Finished processing SD Misu <LIST/> : FAIL code=8192. 

Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE 

Panel A: Reason is unknown,Operation stopped by user. Le processus s

Tuesday, November 25, 2014 11:58:06

1 - Panel A Start processing SD Misu <LIST/>. 

Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="10" onError="" text="Booting hab update firmware.". 

1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="10" onError="" text="Booting hab update firmware." SUCCESS code=0x0. 

Panel A Start <CMD/> type="find" body="Updater" file="" timeout="240" onError="" text="". 

Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE 

Panel A UtpUpdate Event: VolumeArrival Msg: (null) DevState: Updater OpState: WAITING_FOR_DEVICE 

1 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="240" onError="" text="" SUCCESS code=0x0. 

Panel A Start <CMD/> type="push" body="$ echo Programmation" file="" timeout="10" onError="" text="DONE". 

1 - Panel A Finished <CMD/> type="push" body="$ echo Programmation" file="" timeout="10" onError="" text="DONE" FAIL code=0xffffffff. 

Panel A: Operation is not completed.,failed to run command: type="push" body="$ echo Programmation" file="" timeout="10" onError="" text="DONE"   

2 - Panel A Finished processing SD Misu <LIST/> : FAIL code=-1. 

Panel A: Reason is unknown,Operation stopped by user. Le processus s

When I plug my board to the computer, I see the device on mfgtool. I click on "START", the download of the firmware works and the board boots with the linux image.

At the end of the boot, I have this message on mfgtool : Operation is not completed,.,failed to run command: type="push" body="$echo Programmation" file="" timeout="10" onError="" text="DONE"

After that, I have a new "mobile device" on windows device manager. And if click on "STOP3, I see Linux File-Stor Gadget USB Device

Is there someone who knows this problem ?

Linux log :

0x8020a01d

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC

PowerPrep start initialize power...

Battery Voltage = 1.86V

No battery or bad battery                                       detected!!!.Disabling battery                                   vo8

FRAC 0x92925552

memory type is DDR2 - misu

                          Wait for ddr ready 1 -

power 0x00820616

Frac 0x92925552

start change cpu freq

hbus 0x00000003

cpu 0x00010001

start test external memory access

ddr2 0x40000000

finish simple test

LLLLLLLFLCLFLLJUncompressing Linux... done, booting the kernel.

Linux version 2.6.35.3-670-g914558e (victorien@BENNEVIS-VMTUX1204) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #14 Fri Nov 21 16:54:164

CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177

CPU: VIVT data cache, VIVT instruction cache

Machine: Ophrys Systemes Misu board rev002

Memory policy: ECC disabled, Data cache writeback

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 16256

Kernel command line: -e console=ttyAM0,115200 rdinit=/linuxrc rw gpmi

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory: 64MB = 64MB total

Memory: 55328k/55328k available, 10208k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfde00000 - 0xffe00000   (  32 MB)

    vmalloc : 0xc4800000 - 0xf0000000   ( 696 MB)

    lowmem  : 0xc0000000 - 0xc4000000   (  64 MB)

    modules : 0xbf000000 - 0xc0000000   (  16 MB)

      .init : 0xc0008000 - 0xc0027000   ( 124 kB)

      .text : 0xc0027000 - 0xc0305000   (2936 kB)

      .data : 0xc0306000 - 0xc0324dc0   ( 124 kB)

SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Hierarchical RCU implementation.

        RCU-based detection of stalled CPUs is disabled.

        Verbose stalled-CPUs detection is disabled.

NR_IRQS:288

Console: colour dummy device 80x30

console [ttyAM0] enabled

Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

regulator: core version 0.5

NET: Registered protocol family 16

regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal

regulator: vdddbo: 800 <--> 1575 mV fast normal

regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal

vddio = 3380000, val=10

regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal

regulator: overall_current: fast normal

regulator: vbus5v:

regulator: mxs-duart-1: fast normal

regulator: mxs-bl-1: fast normal

regulator: mxs-i2c-1: fast normal

regulator: mmc_ssp-1: fast normal

regulator: mmc_ssp-2: fast normal

regulator: charger-1: fast normal

regulator: power-test-1: fast normal

regulator: cpufreq-1: fast normal

i.MX IRAM pool: 124 KB@0xc4820000

usb DR wakeup device is registered

IMX usb wakeup probe

audit: cannot initialize inotify handle

bio: create slab <bio-0> at 0

SCSI subsystem initialized

Switching to clocksource mxs clock source

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 6144K

Bus freq driver module loaded

mxs_cpu_init: cpufreq init finished

audit: initializing netlink socket (disabled)

type=2000 audit(2.100:1): initialized

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 120

Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)

io scheduler noop registered (default)

Console: switching to colour frame buffer device 100x30

mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART

mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0

Found APPUART 3.1.0

mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1

Found APPUART 3.1.0

mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2

Found APPUART 3.1.0

mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3

Found APPUART 3.1.0

mxs-auart.4: ttySP4 at MMIO 0x80072000 (irq = 116) is a mxs-auart.4

Found APPUART 3.1.0

brd: module loaded

loop: module loaded

Loading iSCSI transport class v2.0-870.

i.MX GPMI NFC

NFC: Version 1, 8-chip GPMI and BCH

Boot ROM: Version 1, Single-chip boot area, block mark swapping supported

Scanning for NAND Flash chips...

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [send_command] DMA error

gpmi-nfc gpmi-nfc.0: [mil_cmd_ctrl] Chip: 0, Error -110

    Command Bytes: 90 00

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

gpmi-nfc gpmi-nfc.0: [gpmi_nfc_dma_go] Chip: 0, DMA Channel: 4, Error -110

gpmi-nfc gpmi-nfc.0: [read_data] DMA error

No NAND device found.

gpmi-nfc gpmi-nfc.0: Chip scan failed

ARC USBOTG Device Controller driver (1 August 2005)

check_parameters:UTP settings are in place now, overriding defaults

g_file_storage gadget: File-backed Storage Gadget, version: 20 November 2008

g_file_storage gadget: Number of LUNs=1

fsl-usb2-udc: bind to driver g_file_storage

mice: PS/2 mouse device common for all mice

input: mxs-kbd as /devices/platform/mxs-kbd.0/input/input0

input: MXS touchscreen as /devices/virtual/input/input1

MXS RTC driver v1.0 hardware v2.3.0

mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0

WARNING : No battery connected !

Aborting power driver initialization

mxs-battery: probe of mxs-battery.0 failed with error 1

mxs-mmc: MXS SSP Controller MMC Interface driver

mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96

mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:01:27 UTC (87)

Freeing init memory: 124K

mmc0: new high speed SDHC card at address 0002

mmcblk0: mmc0:0002 00000 7.41 GiB

mmcblk0:

Starting UTP

ln: /etc/mtab: File exists

disable turn off display

uuc 0.4 [built Nov 18 2014 11:50:23]

UTP: Waiting for device to appear

utp_mk_devnode: creating node '/dev/utp' with 10+222

cpu_id is 28

g_file_storage gadget: high speed config #1

                                           

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,800件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

  You may try to clear SD card under Linux, using dd command :
 

$ sudo dd if=/dev/zero of=/dev/sdb bs=1M count=100

2.

  Please check if USB3 is used on Your host PC. Some issues were

observed with USB3 and MFG.


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,800件の閲覧回数
victorien
Contributor IV

Your answer 1 is correct. This issue appended when I tested the formating of the SD card with mfgtool. And when I rebooted I still have partition on sd card that was use for  mass storage

0 件の賞賛
返信