iMX280 : eliminate a capacitance to GND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX280 : eliminate a capacitance to GND

Jump to solution
749 Views
koichisakagami
Contributor II

Dear community,

I design a custom board with i.MX280 .
As I hope to make the board as small as possible,
I would like to eliminate an unnecessary  capacitance to GND.

In the case of no battery and external loaded device connect with VDD4P2 pin,
Can I eliminate the 33uF capacitance to GND ?
Then the VDD4P2 pin connect to BATTERY and DCDC_BATT via a 1k resistor.

The VDD1P5 pin is same situation.
Can I eliminate the 33uF capacitance with VDD1P5 pin to GND ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
549 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

if these power pins are not used at all, one can eliminate

connected to them capacitors. If one uses "5V only schematic"

capacitor at VDD4P2 should be preserved, since VDD4P2 power is used.

5V only.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
550 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

if these power pins are not used at all, one can eliminate

connected to them capacitors. If one uses "5V only schematic"

capacitor at VDD4P2 should be preserved, since VDD4P2 power is used.

5V only.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply