mfgtool does not burn images after secure boot fusing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool does not burn images after secure boot fusing

1,030 Views
cjej1004
Contributor II

Our lab is currently developing a payment device using imx6ul.

We use the provided mfgtool to burn to eMMC such as u-boot and kernel.

After fusing values for setting the SRK and secure boot mode on the Imx6ul , image burn will not be performed on the eMMC .

Detailed symptom is that the BootStrap state, which loads required files such as u-boot and kernel, is not a conversion to the actual Updater state.

(Xml, Jumping to OS image. Message output only progresses and stops)

If you set the SRK and secure boot mode to Imx6ul, is the current symptom that prevents eMMC from being detected in Windows using mfgtool?

If it is normal, we ask if there is any other way to burn images such as u-boot and kernel after fusing.

Labels (1)
0 Kudos
Reply
1 Reply

909 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX fuses may be burned only once.  It is not possible to burn the fuses, which were burnt previously
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply