mfg_tool, downloading issue, blocked at partition detect?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfg_tool, downloading issue, blocked at partition detect?

Jump to solution
2,690 Views
hubbleye
Contributor I

Hi All,

My board is designed to use sd4 port as eMMC device port, using mfg_tool(Rel-4.1.0_130816) to download images.

When mfg_tool shows jumping to os image, it blocked, seconds later the mfg_tool says no device connected.

I thought the kernel at this step is still running in DDR(ramdisk), not the real eMMC, as before starting kernel, it builds ramdisk area  as follow:

## initrd_high = 0xffffffff, copy_to_ram = 0

in-place initrd

ramdisk load start = 0x12c00040, ramdisk load end = 0x132a90d9

Using Device Tree in place at 18000000, end 1800e6fd

Initial value for argc=3

Final value for argc=3

## Transferring control to Linux (at address 10008000)...

Starting kernel ...

Then i can't figure what is what is wrong, the ramdisk file system, or the eMMC?

*here it begins//////////////////////////////////////////////

U-Boot 2013.04-imx_v2013.04_3.10.17_1.0.0_ga+g06dd4f7 (Dec 30 2014 - 15:37:25)

U-Boot code: 17800000 -> 17854260 BSS: -> 1789B38C

CPU: Freescale i.MX6Q rev1.5 at 792 MHz

Thermal sensor with ratio = 180

CPU: Temperature 34 C, calibration data: 0x5734c17d

Reset cause: POR

Board: MX6Q/SDL-SabreSD

I2C: ready

monitor len: 0009B38C

ramsize: 40000000

TLB table from 4fff0000 to 4fff4000

Top of RAM usable for U-Boot at: 4fff0000

Reserving 620k for U-Boot at: 4ff54000

Reserving 10248k for malloc() at: 4f552000

Reserving 32 Bytes for Board Info at: 4f551fe0

Reserving 176 Bytes for Global Data at: 4f551f30

New Stack Pointer is: 4f551f20

DRAM: 1 GiB

relocation Offset is: 38754000

dram_bank_mmu_setup: bank: 0

monitor flash len: 0005BF68

Now running in RAM - U-Boot at: 4ff54000

CONFIG_GENERIC_MMC start

MMC: case 2 start

case 2 set

before fsl_esdhc_initialize

after fsl_esdhc_initialize

FSL_SDHC: 0

CONFIG_GENERIC_MMC end

MMC Device 1 not found

No MMC card found

Using default environment

Destroy Hash Table: 4ff9ae44 table = 00000000

Create Hash Table: N=304

INSERT: table 4ff9ae44, filled 1/307 rv 4f552cc0 ==> name="bootcmd" value="mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi"

INSERT: table 4ff9ae44, filled 2/307 rv 4f553ee0 ==> name="bootdelay" value="1"

INSERT: table 4ff9ae44, filled 3/307 rv 4f553b5c ==> name="baudrate" value="115200"

INSERT: table 4ff9ae44, filled 4/307 rv 4f552b6c ==> name="ethprime" value="FEC"

INSERT: table 4ff9ae44, filled 5/307 rv 4f552be4 ==> name="loadaddr" value="0x12000000"

INSERT: table 4ff9ae44, filled 6/307 rv 4f55324c ==> name="mfgtool_args" value="setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off "

INSERT: table 4ff9ae44, filled 7/307 rv 4f552ae0 ==> name="initrd_addr" value="0x12C00000"

INSERT: table 4ff9ae44, filled 8/307 rv 4f552e78 ==> name="initrd_high" value="0xffffffff"

INSERT: table 4ff9ae44, filled 9/307 rv 4f5532ec ==> name="bootcmd_mfg" value="run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};"

INSERT: table 4ff9ae44, filled 10/307 rv 4f553490 ==> name="script" value="boot.scr"

INSERT: table 4ff9ae44, filled 11/307 rv 4f552ff4 ==> name="uimage" value="uImage"

INSERT: table 4ff9ae44, filled 12/307 rv 4f553e2c ==> name="fdt_file" value="imx6q-sabresd.dtb"

INSERT: table 4ff9ae44, filled 13/307 rv 4f5538dc ==> name="fdt_addr" value="0x18000000"

INSERT: table 4ff9ae44, filled 14/307 rv 4f553724 ==> name="boot_fdt" value="try"

INSERT: table 4ff9ae44, filled 15/307 rv 4f5540ac ==> name="ip_dyn" value="yes"

INSERT: table 4ff9ae44, filled 16/307 rv 4f552928 ==> name="console" value="ttymxc0"

INSERT: table 4ff9ae44, filled 17/307 rv 4f552a18 ==> name="fdt_high" value="0xffffffff"

INSERT: table 4ff9ae44, filled 17/307 rv 4f552e78 ==> name="initrd_high" value="0xffffffff"

DELETE CANDIDATE: ""

hdelete: DELETE key ""

DELETE ERROR ##############################

INSERT: table 4ff9ae44, filled 18/307 rv 4f552c84 ==> name="mmcpart" value="1"

INSERT: table 4ff9ae44, filled 19/307 rv 4f553b84 ==> name="mmcroot" value="/dev/mmcblk0p2 rootwait rw"

DELETE CANDIDATE: "smp"

hdelete: DELETE key "smp"

DELETE ERROR ##############################

INSERT: table 4ff9ae44, filled 20/307 rv 4f554034 ==> name="mmcargs" value="setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}"

INSERT: table 4ff9ae44, filled 21/307 rv 4f553f80 ==> name="loadbootscript" value="fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};"

INSERT: table 4ff9ae44, filled 22/307 rv 4f5537b0 ==> name="bootscript" value="echo Running bootscript from mmc ...; source"

INSERT: table 4ff9ae44, filled 23/307 rv 4f5529a0 ==> name="loaduimage" value="fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}"

INSERT: table 4ff9ae44, filled 24/307 rv 4f5529f0 ==> name="loadfdt" value="fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}"

INSERT: table 4ff9ae44, filled 25/307 rv 4f553030 ==> name="mmcboot" value="echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;"

INSERT: table 4ff9ae44, filled 26/307 rv 4f553b70 ==> name="netargs" value="setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp"

INSERT: table 4ff9ae44, filled 27/307 rv 4f552a7c ==> name="netboot" value="echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;"

INSERT: free(data = 4f552138)

INSERT: done

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

ipu_clk = 264000000

ldb_clk = 65000000

read BS_CLKGEN0 div:0, final_rate:4224000000, prate:264000000

read BS_CLKGEN0 div:0, final_rate:4224000000, prate:264000000

IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxcfb_init_fbinfo: 4 640 112 524

Framebuffer structures at: fbi=0x4f552138 mxcfbi=0x4f552348

allocated fb @ paddr=0x4F5549E0, size=3145728.

Channel already disabled 9

Channel already uninitialized 9

setup_disp_channel1 called

bpp_to_pixfmt: 16

init channel = 9

pixclock = 64998000l Hz

panel size = 1024 x 768

pixel clk = 64998000

read BS_CLKGEN0 div:0, final_rate:1040000000, prate:65000000

setup_disp_channel2: 95ffcff 1024 768 2048 4f5549e0 4f6d49e0

bpp_to_pixfmt: 16

initializing idma ch 23 @ 027005c0

IPU DMFC DP HIGH RES: 1(0,1), 5B(2~5), 5F(6,7)

IPU_CONF = 0x00000660

IDMAC_CONF = 0x0000002F

IDMAC_CHA_EN1 = 0x00800000

IDMAC_CHA_EN2 = 0x00000000

IDMAC_CHA_PRI1 = 0x18800000

IDMAC_CHA_PRI2 = 0x00000000

IPU_CHA_DB_MODE_SEL0 = 0x00800000

IPU_CHA_DB_MODE_SEL1 = 0x00000000

DMFC_WR_CHAN = 0x00000090

DMFC_WR_CHAN_DEF = 0x202020F6

DMFC_DP_CHAN = 0x0000968A

DMFC_DP_CHAN_DEF = 0x2020F6F6

DMFC_IC_CTRL = 0x00000002

IPU_FS_PROC_FLOW1 = 0x00000000

IPU_FS_PROC_FLOW2 = 0x00000000

IPU_FS_PROC_FLOW3 = 0x00000000

IPU_FS_DISP_FLOW1 = 0x00000000

Framebuffer at 0x4f5549e0

Video: Drawing the logo ...

In: serial

Out: serial

Err: serial

Initial value for argc=3

Final value for argc=3

MMC Device 1 not found

no mmc device at slot 1

Command failed, result=1Net: eth_init: fec_probe(bd, -1, 1) @ 02188000

fec_mii_setspeed: mii_speed 00000014

fec_mdio_read: phy: 01 reg:02 val:0x362

fec_mdio_read: phy: 01 reg:03 val:0x5f24

fec_mii_setspeed: mii_speed 00000014

fec_mdio_read: phy: 01 reg:00 val:0x1140

fec_mdio_write: phy: 01 reg:00 val:0x9140

fec_mdio_read: phy: 01 reg:00 val:0x1140

FEC connected to Generic PHY

fec_mdio_write: phy: 01 reg:0d val:0x7

fec_mdio_write: phy: 01 reg:0e val:0x8016

fec_mdio_write: phy: 01 reg:0d val:0x4007

fec_mdio_read: phy: 01 reg:0e val:0x0

fec_mdio_write: phy: 01 reg:0e val:0x18

fec_mdio_write: phy: 01 reg:1d val:0x5

fec_mdio_read: phy: 01 reg:1e val:0x0

fec_mdio_write: phy: 01 reg:1e val:0x100

fec_mdio_read: phy: 01 reg:01 val:0x7949

fec_mdio_read: phy: 01 reg:0f val:0x3000

fec_mdio_read: phy: 01 reg:04 val:0xde1

fec_mdio_write: phy: 01 reg:04 val:0x1e1

fec_mdio_read: phy: 01 reg:09 val:0xf00

fec_mdio_read: phy: 01 reg:00 val:0x1140

fec_mdio_write: phy: 01 reg:00 val:0x1340

Initial value for argc=3

Final value for argc=3

FEC [PRIME]

Warning: failed to set MAC address

Boot from USB for mfgtools

Use default environment for mfgtools

Destroy Hash Table: 4ff9ae44 table = 4f5528c0

Create Hash Table: N=304

INSERT: table 4ff9ae44, filled 1/307 rv 4f552b98 ==> name="bootcmd" value="mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi"

INSERT: table 4ff9ae44, filled 2/307 rv 4f553db8 ==> name="bootdelay" value="1"

INSERT: table 4ff9ae44, filled 3/307 rv 4f553a34 ==> name="baudrate" value="115200"

INSERT: table 4ff9ae44, filled 4/307 rv 4f552a44 ==> name="ethprime" value="FEC"

INSERT: table 4ff9ae44, filled 5/307 rv 4f552abc ==> name="loadaddr" value="0x12000000"

INSERT: table 4ff9ae44, filled 6/307 rv 4f553124 ==> name="mfgtool_args" value="setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off "

INSERT: table 4ff9ae44, filled 7/307 rv 4f5529b8 ==> name="initrd_addr" value="0x12C00000"

INSERT: table 4ff9ae44, filled 8/307 rv 4f552d50 ==> name="initrd_high" value="0xffffffff"

INSERT: table 4ff9ae44, filled 9/307 rv 4f5531c4 ==> name="bootcmd_mfg" value="run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};"

INSERT: table 4ff9ae44, filled 10/307 rv 4f553368 ==> name="script" value="boot.scr"

INSERT: table 4ff9ae44, filled 11/307 rv 4f552ecc ==> name="uimage" value="uImage"

INSERT: table 4ff9ae44, filled 12/307 rv 4f553d04 ==> name="fdt_file" value="imx6q-sabresd.dtb"

INSERT: table 4ff9ae44, filled 13/307 rv 4f5537b4 ==> name="fdt_addr" value="0x18000000"

INSERT: table 4ff9ae44, filled 14/307 rv 4f5535fc ==> name="boot_fdt" value="try"

INSERT: table 4ff9ae44, filled 15/307 rv 4f553f84 ==> name="ip_dyn" value="yes"

INSERT: table 4ff9ae44, filled 16/307 rv 4f552800 ==> name="console" value="ttymxc0"

INSERT: table 4ff9ae44, filled 17/307 rv 4f5528f0 ==> name="fdt_high" value="0xffffffff"

INSERT: table 4ff9ae44, filled 17/307 rv 4f552d50 ==> name="initrd_high" value="0xffffffff"

DELETE CANDIDATE: ""

hdelete: DELETE key ""

DELETE ERROR ##############################

INSERT: table 4ff9ae44, filled 18/307 rv 4f552b5c ==> name="mmcpart" value="1"

INSERT: table 4ff9ae44, filled 19/307 rv 4f553a5c ==> name="mmcroot" value="/dev/mmcblk0p2 rootwait rw"

DELETE CANDIDATE: "smp"

hdelete: DELETE key "smp"

DELETE ERROR ##############################

INSERT: table 4ff9ae44, filled 20/307 rv 4f553f0c ==> name="mmcargs" value="setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}"

INSERT: table 4ff9ae44, filled 21/307 rv 4f553e58 ==> name="loadbootscript" value="fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};"

INSERT: table 4ff9ae44, filled 22/307 rv 4f553688 ==> name="bootscript" value="echo Running bootscript from mmc ...; source"

INSERT: table 4ff9ae44, filled 23/307 rv 4f552878 ==> name="loaduimage" value="fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}"

INSERT: table 4ff9ae44, filled 24/307 rv 4f5528c8 ==> name="loadfdt" value="fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}"

INSERT: table 4ff9ae44, filled 25/307 rv 4f552f08 ==> name="mmcboot" value="echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;"

INSERT: table 4ff9ae44, filled 26/307 rv 4f553a48 ==> name="netargs" value="setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp"

INSERT: table 4ff9ae44, filled 27/307 rv 4f552954 ==> name="netboot" value="echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;"

INSERT: free(data = 4f8549e8)

INSERT: done

### main_loop entered: bootdelay=0

Run bootcmd_mfg: run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};

### main_loop: bootcmd="run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};"

Hit any key to stop autoboot: 0

Initial value for argc=10

Final value for argc=10

## Current stack ends at 0x4f551c98 * kernel: cmdline image address = 0x12000000

## Booting kernel from Legacy Image at 12000000 ...

  Image Name: Linux-3.10.17-1.0.2_ga-mfgtool+g

  Image Type: ARM Linux Kernel Image (uncompressed)

  Data Size: 5260312 Bytes = 5 MiB

  Load Address: 10008000

  Entry Point: 10008000

  Verifying Checksum ... OK

  kernel data at 0x12000040, len = 0x00504418 (5260312)

* ramdisk: cmdline image address = 0x12c00000

## Loading init Ramdisk from Legacy Image at 12c00000 ...

  Image Name: fsl-image-mfgtool-initramfs-cmt_

  Image Type: ARM Linux RAMDisk Image (gzip compressed)

  Data Size: 6983833 Bytes = 6.7 MiB

  Load Address: 00000000

  Entry Point: 00000000

  Verifying Checksum ... OK

  ramdisk start = 0x12c00040, ramdisk end = 0x132a90d9

* fdt: cmdline image address = 0x18000000

## Checking for 'FDT'/'FDT Image' at 18000000

* fdt: raw FDT blob

## Flattened Device Tree blob at 18000000

  Booting using the fdt blob at 0x18000000

  of_flat_tree at 0x18000000 size 0x0000b6fe

Initial value for argc=3

Final value for argc=3

  Loading Kernel Image ... OK

OK

  kernel loaded at 0x10008000, end = 0x1050c418

Read SW1AB error!

using: FDT

using: FDT

## initrd_high = 0xffffffff, copy_to_ram = 0

  in-place initrd

  ramdisk load start = 0x12c00040, ramdisk load end = 0x132a90d9

  Using Device Tree in place at 18000000, end 1800e6fd

Initial value for argc=3

Final value for argc=3

## Transferring control to Linux (at address 10008000)...

Starting kernel ...

Booting Linux on physical CPU 0x0

Linux version 3.10.17-1.0.2_ga-mfgtool+g33597e3 (liuzh@liuzh) (gcc version 4.9.1 (GCC) ) #5 SMP Sun Jan 4 11:53:03 CST 2015

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board

cma: CMA: reserved 256 MiB at 40000000

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @81518000 s8704 r8192 d15872 u32768

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096

Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 1024MB = 1024MB total

Memory: 756504k/756504k available, 292072k reserved, 0K highmem

Virtual kernel memory layout:

  vector : 0xffff0000 - 0xffff1000 ( 4 kB)

  fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)

  vmalloc : 0xc0800000 - 0xff000000 (1000 MB)

  lowmem : 0x80000000 - 0xc0000000 (1024 MB)

  modules : 0x7f000000 - 0x80000000 ( 16 MB)

  .text : 0x80008000 - 0x80c00460 (12258 kB)

  .init : 0x80c01000 - 0x80c4c200 ( 301 kB)

  .data : 0x80c4e000 - 0x80c9d3e0 ( 317 kB)

  .bss : 0x80c9d3e0 - 0x80d0015c ( 396 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6Q, silicon rev 1.5

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x80634de8 - 0x80634e40

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG2 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1125 mV

vdd3p0: 2800 <--> 3150 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2425 mV

cpu: 725 <--> 1450 mV at 1150 mV

vddpu: 725 <--> 1450 mV

vddsoc: 725 <--> 1450 mV at 1200 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

usb_otg_vbus: 5000 mV

usb_h1_vbus: 5000 mV

wm8962-supply: no parameters

mipi_dsi_pwr_on: no parameters

sensor-supply: 3300 mV

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

i2c i2c-2: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

cfg80211: Calling CRDA to update world regulatory domain

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 6816K (82c01000 - 832a9000)

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

pureg-dummy: no parameters

imx6_busfreq busfreq.15: DDR medium rate not supported.

Bus freq driver module loaded

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 2002

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: WEIM driver registered.

mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

mxc_sdc_fb fb.30: register mxc display driver ldb

imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_sdc_fb fb.31: register mxc display driver hdmi

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

fbcvt: 1920x1080@60: CVT Name - 2.073M9

mxc_sdc_fb fb.32: register mxc display driver lcd

mxc_sdc_fb fb.32: ipu0-di0 already in use

mxc_sdc_fb: probe of fb.32 failed with error -16

mxc_sdc_fb fb.33: register mxc display driver ldb

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: loaded firmware 1.1

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 1-0008: unrecognized pfuze chip ID!

pfuze100-regulator: probe of 1-0008 failed with error -5

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled

serial: Freescale lpuart driver

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

Wait for CR ACK error!

sata phy RX_PLL is stable!

ahci: SSS flag set, parallel bus scan disabled

ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode

ahci ahci: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst

scsi0 : ahci_platform

ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71

m25p80 spi32766.0: found m25p128, expected m25p32

m25p80 spi32766.0: m25p128 (16384 Kbytes)

spi_imx 2008000.ecspi: probed

fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00

fec 2188000.ethernet (unregistered net_device): Using random MAC address: 2a:a2:65:06:6d:9f

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 3.10.17-1.0.2_ga-mfgtool+g33597e3 ehci_hcd

usb usb1: SerialNumber: ci_hdrc.1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

elan-touch 2-0010: elan - Read Hello Packet Failed

elan-touch: probe of 2-0010 failed with error -22

egalax_ts 1-0004: Failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

ata1: SATA link down (SStatus 0 SControl 300)

egalax_ts 2-0004: Failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video17

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video18

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video19

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video20

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

mag3110 2-000e: check mag3110 chip ID

mag3110 2-000e: read chip ID 0xffffff92 is not equal to 0xc4!

mag3110: probe of 2-000e failed with error -22

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!

mma8451: probe of 0-001c failed with error -22

imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc0: no vqmmc regulator found

mmc0: no vmmc regulator found

mmc0: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz

Galcore version 4.6.9.9754

galcore options:

  irqLine = 41

  registerMemBase = 0x00130000

  registerMemSize = 0x00004000

mmc0: new high speed DDR MMC card at address 0001

mmcblk0: mmc0:0001 SEM08G 7.39 GiB

mmcblk0boot0: mmc0:0001 SEM08G partition 1 1.00 MiB

mmcblk0boot1: mmc0:0001 SEM08G partition 2 1.00 MiB

mmcblk0rpmb: mmc0:0001 SEM08G partition 3 128 KiB

mmcblk0: p1

mmcblk0boot1: unknown partition table

mmcblk0boot0: unknown partition table

Labels (3)
0 Kudos
Reply
1 Solution
2,257 Views
igorpadykov
NXP Employee
NXP Employee

Hi hubble

for new board MFG Tool firmware should be rebuilt to take into account

board specifics (for example different DDR configuration/calibration settings),

please use "fsl-image-mfgtool-initramfs" as target recipe

for obtaining source code for mfgtool linux kernel.

Note that new board DDR calibration settings should be obtained from DDR tests

i.MX6 DDR Stress Test Tool V1.0.3

Best regards

igor

View solution in original post

0 Kudos
Reply
1 Reply
2,258 Views
igorpadykov
NXP Employee
NXP Employee

Hi hubble

for new board MFG Tool firmware should be rebuilt to take into account

board specifics (for example different DDR configuration/calibration settings),

please use "fsl-image-mfgtool-initramfs" as target recipe

for obtaining source code for mfgtool linux kernel.

Note that new board DDR calibration settings should be obtained from DDR tests

i.MX6 DDR Stress Test Tool V1.0.3

Best regards

igor

0 Kudos
Reply