mfg tool - bootstrap and updater

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mfg tool - bootstrap and updater

跳至解决方案
1,277 次查看
rans
Senior Contributor I

Hello,

I would please like to ask a question about mfg tool.

I've read the documentation of mfg tool, and would please like to know:

1. According to documentation it requires that we dedicated u-boot & kernel for mfg tool, are these binaries should be programmed to the same storage device as the "updater" u-boot/kernel ?

2. When we update u-boot/kernel (updater), does it override the u-boot/kernel for mfg/tool ? If yes - why can't we use the u-boot/kernel for mfg tool, as  operational firmware u-boot/kernel ? (in such way we don't need the updater)

Best Regards,

Ran

0 项奖励
回复
1 解答
1,077 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ran

files which uses mfg tools (it is its own image) are located in

..OS Firmware/firmware folder, files which will be programmed

to media (programmed to some storage device) - in ..OS Firmware/files

folder, also it is useful to check documents in /Document folder. Default

u-boot/kernel for mfg/tool is built for nxp reference boards, for custom board it

should be rebuilt, if custom board is identical to reference board, it may work

without rebuilding firmware files.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,078 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ran

files which uses mfg tools (it is its own image) are located in

..OS Firmware/firmware folder, files which will be programmed

to media (programmed to some storage device) - in ..OS Firmware/files

folder, also it is useful to check documents in /Document folder. Default

u-boot/kernel for mfg/tool is built for nxp reference boards, for custom board it

should be rebuilt, if custom board is identical to reference board, it may work

without rebuilding firmware files.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复