mek_8q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mek_8q

2,713 次查看
ilanganor1
Contributor III

I am using IMX8 EVK 

flashed Android 11 on SD card, and testing suspend to RAM

device enters suped to RAM and exit OK

but power meaasurments are very hugh (X10 then expected)

according to measurments board 2 HDMI inputs phy are on even in suspend to RAM

1. please advice how to disable that

2. please indicate if Android 11 default image should reach the datasheet suspend to RAM power consumption performance

 

0 项奖励
回复
4 回复数

2,695 次查看
ilanganor1
Contributor III

1. how can I reach lowest power in suspend to RAM using Android + IMX8PEVK? 

2. I think most power consumption is due to HDMI PHY, how can I shut it down before going to suspend to RAM? 

0 项奖励
回复

2,688 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

 

>how can I reach lowest power in suspend to RAM using Android + IMX8PEVK?

 

nxp has special service for perform various optimizatons:

https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 项奖励
回复

2,702 次查看
igorpadykov
NXP Employee
NXP Employee

Hi גנור

 

higher power consumption may be due to leakage, may be recommended to look

at AN13249: i.MX 8QuadMax Current Drain with Low- and High-Power Use Cases

 

>2. please indicate if Android 11 default image should reach the datasheet suspend to RAM power consumption performance

 

no

 

Best regards
igor

0 项奖励
回复

2,694 次查看
ilanganor1
Contributor III

1. how can I reach lowest power in suspend to RAM using Android + IMX8PEVK? 

2. I think most power consumption is due to HDMI PHY, how can I shut it down before going to suspend to RAM? 

 

 

0 项奖励
回复