mcimx6ull_evk ... I'm an absolute beginner

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcimx6ull_evk ... I'm an absolute beginner

4,002件の閲覧回数
fabio_poiatti
Contributor III

Hi

I'm Fabio and I'm a beginner about linux environment .

Now I'm involved in some new development and we bought the mcimx6ull_evk for some experiments.

Where can I find some description about the BSP for imx.6 ULL?

I saw the sd card coming with the EVK has a structure like 2 partitions (one for the image and one for the 

classic environment) but if I download a new BSP I find only the image and not the directory structure...???

How can I write the new BSP on sd card?

many thaks

Fabio

ps I tried to find these information on the community with serach tab but without any success :-(

10 返答(返信)

3,417件の閲覧回数
joe_schneider
Contributor I

+1

I also ran into the same issues as stated above. The demo images stated to boot on the i.MX6 ULL EVK do NOT boot or crash. I wasted time thinking this was a faster way to my goals, then I need to waste more time to build a non-customized kernel/rootfs that should be generally available. This seems like something NXP should fix.

0 件の賞賛
返信

3,418件の閲覧回数
fabio_poiatti
Contributor III

thanks to all

I resolved by a toolchain installation with creation of a new kernel from Yocto project

0 件の賞賛
返信

3,418件の閲覧回数
fabio_poiatti
Contributor III

I tried two old versions of BSP and both starts .... so my procedure to create a bootable SD CARD is correct ...

But both end with failure ... this is the log

BSP version L4.9.88_2.0.0_MX6UL7D

U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (May 01 2018 - 04:23:58 -0)

CPU: Freescale i.MX6ULL rev1.0 528 MHz (running at 396 MHz)

CPU: Commercial temperature grade (0C to 95C) at 43C

Reset cause: POR

Model: Freescale i.MX6 UltraLite 14x14 EVK Board

Board: MX6UL 14x14 EVK

DRAM: 512 MiB

MMC: FSL_SDHC: 0, FSL_SDHC: 1

*** Warning - bad CRC, using default environment

Display: TFT43AB (480x272)

Video: 480x272x24

In: serial

Out: serial

Err: serial

switch to partitions #0, OK

mmc1 is current device

Net:

Warning: ethernet@020b4000 using MAC address from ROM

eth1: ethernet@020b4000 [PRIME]

Warning: ethernet@02188000 using MAC address from ROM

, eth0: ethernet@02188000

Normal Boot

Hit any key to stop autoboot: 0

switch to partitions #0, OK

mmc1 is current device

switch to partitions #0, OK

mmc1 is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

7493456 bytes read in 345 ms (20.7 MiB/s)

Booting from mmc ...

reading imx6ul-14x14-evk.dtb

37340 bytes read in 27 ms (1.3 MiB/s)

Kernel image @ 0x80800000 [ 0x000000 - 0x725750 ]

## Flattened Device Tree blob at 83000000

Booting using the fdt blob at 0x83000000

Using Device Tree in place at 83000000, end 8300c1db

Modify /soc/aips-bus@02100000/sim@0218c000:status disabled

ft_system_setup for mx6

Starting kernel ...

Booting Linux on physical CPU 0x0

Linux version 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d (oe-user@oe-host) (gcc versio8

CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d

CPU: div instructions available: patching division code

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

OF: fdt:Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board

Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB

OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool

Memory policy: Data cache writealloc

percpu: Embedded 14 pages/cpu @8bb31000 s25996 r8192 d23156 u57344

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 175848K/524288K available (9216K kernel code, 577K rwdata, 3388K rodata)

Virtual kernel memory layout:

vector : 0xffff0000 - 0xffff1000 ( 4 kB)

fixmap : 0xffc00000 - 0xfff00000 (3072 kB)

vmalloc : 0xa0800000 - 0xff800000 (1520 MB)

lowmem : 0x80000000 - 0xa0000000 ( 512 MB)

pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)

modules : 0x7f000000 - 0x7fe00000 ( 14 MB)

.text : 0x80008000 - 0x80a00000 (10208 kB)

.init : 0x80e00000 - 0x80f00000 (1024 kB)

.data : 0x80f00000 - 0x80f904e0 ( 578 kB)

.bss : 0x80f92000 - 0x81008a38 ( 475 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

Build-time adjustment of leaf fanout to 32.

RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.

RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1

NR_IRQS:16 nr_irqs:16 16

Switching to timer-based delay loop, resolution 333ns

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns

clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: s

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)

Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)

CPU: Testing write buffer coherency: ok

/cpus/cpu@0 missing clock-frequency property

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x80100000 - 0x80100058

Brought up 1 CPUs

SMP: Total of 1 processors activated (6.00 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5

clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 191s

futex hash table entries: 256 (order: 2, 16384 bytes)

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor menu

hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 8 bytes.

imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

mxs-dma 1804000.dma-apbh: initialized

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-0: can't use DMA, using PIO instead.

i2c i2c-1: IMX I2C adapter registered

i2c i2c-1: can't use DMA, using PIO instead.

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@>

PTP clock support registered

MIPI CSI2 driver module loaded

imx rpmsg driver is registered.

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.22

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

clocksource: Switched to clocksource mxc_timer1

VFS: Disk quotas dquot_6.6.0

VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NET: Registered protocol family 2

TCP established hash table entries: 4096 (order: 2, 16384 bytes)

TCP bind hash table entries: 4096 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 4096 bind 4096)

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

imx_busfreq soc:busfreq: busfreq_probe failed to get busfreq clk for imx6ull/sl.

imx_busfreq: probe of soc:busfreq failed with error -22

Bus freq driver module loaded

workingset: timestamp_bits=30 max_order=17 bucket_order=0

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.

fuse init (API version 7.26)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: Driver registered.

backlight supply power not found, using dummy regulator

21c8000.lcdif supply lcd not found, using dummy regulator

Console: switching to colour frame buffer device 60x34

mxsfb 21c8000.lcdif: initialized

imx-sdma 20ec000.sdma: loaded firmware 3.3

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a X

console [ttymxc0] enabled

21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 66, base_baud = 5000000) is a X

imx sema4 driver is registered.

[drm] Initialized

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

fsl-quadspi 21e0000.qspi: n25q256a (32768 Kbytes)

spi_gpio spi4: gpio-miso property not found, switching to no-rx mode

libphy: Fixed MDIO Bus: probed

CAN device driver interface

flexcan 2090000.flexcan: device registered (reg_base=a09a4000, irq=25)

flexcan 2094000.flexcan: device registered (reg_base=a09ac000, irq=26)

20b4000.ethernet supply phy not found, using dummy regulator

pps pps0: new PPS source ptp0

libphy: fec_enet_mii_bus: probed

fec 20b4000.ethernet eth0: registered PHC device 0

2188000.ethernet supply phy not found, using dummy regulator

pps pps1: new PPS source ptp1

fec 2188000.ethernet eth1: registered PHC device 1

usbcore: registered new interface driver kaweth

pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver

usbcore: registered new interface driver pegasus

usbcore: registered new interface driver rtl8150

usbcore: registered new interface driver r8152

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usb_ehset_test

2184800.usbmisc supply vbus-wakeup not found, using dummy regulator

2184000.usb supply vbus not found, using dummy regulator

2184200.usb supply vbus not found, using dummy regulator

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

input: 20cc000.snvs:snvs-powerkey as /devices/soc0/soc/2000000.aips-bus/20cc0000

input: iMX6UL Touchscreen Controller as /devices/soc0/soc/2000000.aips-bus/20401

input: FreescaleAccelerometer as /devices/virtual/input/input2

fxls8471 device driver probe successfully

snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as 0

i2c /dev entries driver

IR NEC protocol handler initialized

IR RC5(x/sz) protocol handler initialized

IR RC6 protocol handler initialized

IR JVC protocol handler initialized

IR Sony protocol handler initialized

IR SANYO protocol handler initialized

IR Sharp protocol handler initialized

IR MCE Keyboard/mouse protocol handler initialized

IR XMP protocol handler initialized

pxp-v4l2 pxp_v4l2: initialized

0-000e supply vdd not found, using dummy regulator

0-000e supply vddio not found, using dummy regulator

mag3110 0-000e: check mag3110 chip ID

input: mag3110 as /devices/virtual/input/input3

random: fast init done

mag3110 0-000e: mag3110 is probed

imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)

Bluetooth: HCI UART driver ver 2.3

Bluetooth: HCI UART protocol H4 registered

Bluetooth: HCI UART protocol BCSP registered

Bluetooth: HCI UART protocol ATH3K registered

usbcore: registered new interface driver bcm203x

usbcore: registered new interface driver btusb

usbcore: registered new interface driver ath3k

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA

sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on noe

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

Unhandled fault: external abort on non-linefetch (0x1008) at 0xa0a00fd4

pgd = 80004000

[a0a00fd4] *pgd=884b5811, *pte=02140653, *ppte=02140453

Internal error: : 1008 [#1] PREEMPT SMP ARM

Modules linked in:

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1

Hardware name: Freescale i.MX6 UltraLite (Device Tree)

task: 8804c000 task.stack: 88050000

PC is at caam_probe+0x360/0xcf8

LR is at _raw_spin_unlock_irqrestore+0x28/0x54

pc : [<8077cc94>] lr : [<809eaaa0>] psr: 60000013

sp : 88051e18 ip : 80a2d098 fp : 00000000

r10: 80ff9fc0 r9 : 884afe40 r8 : 00000000

r7 : a0a00000 r6 : 8810b410 r5 : 8810b400 r4 : 88468a10

r3 : a0a00fd4 r2 : 00000000 r1 : 00000001 r0 : 00000000

Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none

Control: 10c53c7d Table: 8000406a DAC: 00000051

Process swapper/0 (pid: 1, stack limit = 0x88050210)

Stack: (0x88051e18 to 0x88052000)

1e00: 00000000 80cf3e8c

1e20: 00000000 8026736c 8810c960 80cf3e8c 00000000 00000001 8810c960 884b17d0

1e40: 00000000 8810c960 80cf3e8c 884b1870 00000001 8810b410 fffffffe 80f6d3d4

1e60: fffffdfb 00000000 00000000 80e75bfc 00000000 804d0a90 8810b410 80ff0420

1e80: 00000000 80f6d3d4 00000000 804cf19c 8810b410 80f6d3d4 8810b444 00000000

1ea0: 00000007 00000159 80e75bfc 804cf32c 00000000 80f6d3d4 804cf288 804cd6ec

1ec0: 8807b15c 881036b4 80f6d3d4 884b4100 80f35cf0 804ce82c 80cdd60c 80e4a52c

1ee0: ffffe000 80f6d3d4 80e4a52c ffffe000 80e6383c 804cfbb8 00000000 80e4a52c

1f00: ffffe000 801017dc 80f0fce4 00000000 cccccccd 8025dd44 80fe2f00 88033b00

1f20: 00000000 80f0e8fc 80a2d098 8bfffab6 00000159 80148f34 80d4c968 80cb60e4

1f40: 80c3098c 00000006 00000006 00000000 80f0e8e4 80f92000 80f92000 80f92000

1f60: 80e63834 80e6383c 00000007 80e75bfc 00000000 80e00da4 00000006 00000006

1f80: 00000000 80e005a8 00000000 809e52f8 00000000 00000000 00000000 00000000

1fa0: 00000000 809e5300 00000000 80107950 00000000 00000000 00000000 00000000

1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

1fe0: 00000000 00000000 00000000 00000000 00000013 00000000 ffffffff ffffffff

[<8077cc94>] (caam_probe) from [<804d0a90>] (platform_drv_probe+0x50/0xac)

[<804d0a90>] (platform_drv_probe) from [<804cf19c>] (driver_probe_device+0x1cc/)

[<804cf19c>] (driver_probe_device) from [<804cf32c>] (__driver_attach+0xa4/0xa8)

[<804cf32c>] (__driver_attach) from [<804cd6ec>] (bus_for_each_dev+0x4c/0x9c)

[<804cd6ec>] (bus_for_each_dev) from [<804ce82c>] (bus_add_driver+0x188/0x20c)

[<804ce82c>] (bus_add_driver) from [<804cfbb8>] (driver_register+0x78/0xf4)

[<804cfbb8>] (driver_register) from [<801017dc>] (do_one_initcall+0x44/0x170)

[<801017dc>] (do_one_initcall) from [<80e00da4>] (kernel_init_freeable+0x158/0x)

[<80e00da4>] (kernel_init_freeable) from [<809e5300>] (kernel_init+0x8/0x110)

[<809e5300>] (kernel_init) from [<80107950>] (ret_from_fork+0x14/0x24)

Code: e5c4005c e5da2000 e2833004 e3520000 (e5933000)

---[ end trace e56ba16ec7d2c12a ]---

Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

mmc1: host does not support reading read-only switch, assuming write-enable

mmc1: new high speed SDHC card at address 0007

mmcblk1: mmc1:0007 SDCIT 7.29 GiB

mmcblk1: p1 p2

Two question:

1) why the L4.14.78_1.0.0 does not start?

2) what does the kernel panic error means?

Many many thanks

0 件の賞賛
返信

3,418件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Fabio,
Welcome to i.MX, Linux and Yocto world. For additional reference, you could take a look to the following Community document, that helps to understand Yocto for future image buildings:

https://community.nxp.com/docs/DOC-94035

Hope this will be useful for you.
Best regards!
/Carlos


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信

3,418件の閲覧回数
fabio_poiatti
Contributor III

thanks but the link give to me the

Unauthorized

response :-(

0 件の賞賛
返信

3,418件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Fabio,

In such case, you could take a look to the following link instead:

Continental Yocto Tutorial / August 2013 

Hope this will be useful for you.
Best regards!
/Carlos


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信

3,418件の閲覧回数
shivanipatel
Senior Contributor II

Hi, fabio mario poiatti

Please refer below-mentioned links for i.MX6ULL EVK board specific Documentations and demo images on different version of BSPs .

To setup a build environment for i.MX6ULL EVK, you can follow this link, in which you will find the document named i.MX_Yocto_Project_User's_Guide.pdf which describes how to build an image for an i.MX6ULL EVK board and  i.MX_Linux_User's_Guide.pdf document provides the steps to flash images on any boot device like SD Card.

Regards,

Shivani Patel

3,418件の閲覧回数
fabio_poiatti
Contributor III

thanks Shivani Patel

I tried exactly the command you suggested but without any success ..

sudo dd if=fsl-image-validation-imx-imx6ul7d.sdcard of=/dev/mmcblk0 bs=1M && sync

Is it enough to flash a new sd card with only the BSP fsl-image-validation-imx-imx6ul7d.sdcard ?

Or it is necessary to flash something else?

You said "The BSP package L4.14.78_1.0.0_ga_images_MX6UL7D.zip contains common SDCARD image for all i.mx6ul, i.mx6ull, and imx7d boards." ... what does it mean? Is that image not correct for my EVK application?

Thanks

0 件の賞賛
返信

3,418件の閲覧回数
fabio_poiatti
Contributor III

Hi,

many thanks for your response.

I'm going to read the documents you indicated ... in the meantime I tried to generate an sd card for a newer

bsp (in respect of the sd card coming with evk) but linux does not start :-(

the red led remain always on

for creation af the new sd card I followed this list of actions:

1) download a new BSP from the NXP website L4.14.78_1.0.0_ga_images_MX6UL7D.zip

2) extract from .zip the file fsl-image-validation-imx-imx6ul7d.sdcard

3) insert a new sd card in the pc slot with adapter

4) sudo dd if=fsl-image-validation-imx-imx6ul7d.sdcard of=/dev/mmcblk0 bs=1M && sync

5) insert the new written sd card in the EVK

6) switch on the EVK remains with red led on

How is it possible to chose between imx6ul imx6ull imx6ulz or imx7d image?

0 件の賞賛
返信

3,418件の閲覧回数
shivanipatel
Senior Contributor II

Hi, fabio.poiatti@softeco.it

Please try below command to flash the SDCARD image,

  • sudo dd if=<image name>.sdcard of=DISK bs=1M && sync
    • Where DISK = /dev/mmcblk0, for a card connected via a PCI card reader
    • And DISK = /dev/sdX, for a card connected via a USB card reader
      • where X stands for your sdcard node label. It could be a/b/c which is determined using lsblk commad.

The BSP package L4.14.78_1.0.0_ga_images_MX6UL7D.zip contains common SDCARD image for all i.mx6ul, i.mx6ull, and imx7d boards.

Regards,

Shivani Patel

0 件の賞賛
返信