max supply current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

max supply current

Jump to solution
3,566 Views
sapirbuz
Contributor IV

Hi,

can you please give me an example of how to calculate the maximum supply current? i didn't understand it from the picture below 

NVCC_EMC(max curr)= 42*C*3.3*0.5F= 69.3CF

please help me estimate C and F

sapirbuz_0-1655661092693.png

 

0 Kudos
Reply
1 Solution
3,521 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

No, C couldn't be 4.9uF. It's impossible to push 42 4.9uF cap to 60M. Please refer to this post.

https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-Max-supply-current/m-p/416445

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
6 Replies
3,558 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

C is the whole capacitor load on the pin group. You can add them all according to your design.

F is signal frequency. For example, if the pin group is for SDRAM, then take the SDRAM working frequency.

 

Regards,

Jing

0 Kudos
Reply
3,556 Views
sapirbuz
Contributor IV

This bank consists 42 pins, what freq should I choose?

what is the maximum freq?

0 Kudos
Reply
3,547 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

This formula can help you to estimate maximum power consumption. It could not be very accurate. So, just use the highest frequency signal. For example, if the highest frequency signal in this group is a SPI, you can use the SPI bus frequency.  

https://community.nxp.com/t5/i-MX-RT/RT1170-Max-Supply-Current-Calculation/td-p/1359582

 

Regards,

Jing

0 Kudos
Reply
3,542 Views
sapirbuz
Contributor IV

Hi,

F= 60MHz (QSPI)

C= 4.9uF (according to eval board)

NVCC_EMC(max curr)= 42*C*3.3*0.5F= 69.3CF= 20374.2A?

what did i miss? 

 

only for QSPI pins:

4*4.9u*3.3*0.5*60M= 1940A

it doesn't make sense

0 Kudos
Reply
3,522 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

No, C couldn't be 4.9uF. It's impossible to push 42 4.9uF cap to 60M. Please refer to this post.

https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-Max-supply-current/m-p/416445

 

Regards,

Jing

0 Kudos
Reply
3,518 Views
sapirbuz
Contributor IV

thank you

0 Kudos
Reply