max supply current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,561件の閲覧回数
sapirbuz
Contributor IV

Hi,

can you please give me an example of how to calculate the maximum supply current? i didn't understand it from the picture below 

NVCC_EMC(max curr)= 42*C*3.3*0.5F= 69.3CF

please help me estimate C and F

sapirbuz_0-1655661092693.png

 

0 件の賞賛
返信
1 解決策
3,516件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

No, C couldn't be 4.9uF. It's impossible to push 42 4.9uF cap to 60M. Please refer to this post.

https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-Max-supply-current/m-p/416445

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,553件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

C is the whole capacitor load on the pin group. You can add them all according to your design.

F is signal frequency. For example, if the pin group is for SDRAM, then take the SDRAM working frequency.

 

Regards,

Jing

0 件の賞賛
返信
3,551件の閲覧回数
sapirbuz
Contributor IV

This bank consists 42 pins, what freq should I choose?

what is the maximum freq?

0 件の賞賛
返信
3,542件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

This formula can help you to estimate maximum power consumption. It could not be very accurate. So, just use the highest frequency signal. For example, if the highest frequency signal in this group is a SPI, you can use the SPI bus frequency.  

https://community.nxp.com/t5/i-MX-RT/RT1170-Max-Supply-Current-Calculation/td-p/1359582

 

Regards,

Jing

0 件の賞賛
返信
3,537件の閲覧回数
sapirbuz
Contributor IV

Hi,

F= 60MHz (QSPI)

C= 4.9uF (according to eval board)

NVCC_EMC(max curr)= 42*C*3.3*0.5F= 69.3CF= 20374.2A?

what did i miss? 

 

only for QSPI pins:

4*4.9u*3.3*0.5*60M= 1940A

it doesn't make sense

0 件の賞賛
返信
3,517件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

No, C couldn't be 4.9uF. It's impossible to push 42 4.9uF cap to 60M. Please refer to this post.

https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-Max-supply-current/m-p/416445

 

Regards,

Jing

0 件の賞賛
返信
3,513件の閲覧回数
sapirbuz
Contributor IV

thank you

0 件の賞賛
返信