max 17059

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

max 17059

1,527 Views
rizwan_s
Contributor II

Hi ,

I am working on imx6 solo custom board with linux yocto. now working on max 17059 fuel guage IC.

its capacity is as follows:

5.5V-0%
7.4V-50%
8.4V-100%

At 8.4V it shows 100% but it shows 0% at 7V only and board will be ON  for 3 to 4 hours even after it shows 0% battery.

How can i solve this issue?

Please suggest

Thanks and Regards

Rizwan Syed

Labels (4)
0 Kudos
Reply
1 Reply

1,425 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

one can check sensor ground connections and software with max 17059 evk and software

MAX17059 1-Cell/2-Cell Fuel Gauge with ModelGauge - Maxim 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply