The attatched image contains error ,plz share the solution to this
Hi @kavyav,
I hope you are doing well.From the image, It is seen that error is with the below statement"make -r -j4 all" terminated with exit code 2. The build might be incomplete.I have a few queries to ask.->Which IMX board are you using?->Have you made any changes to Makefile or are you using the default given SDKI have shared a link to docs please refer to section 5.1 (Build an app using Linux host) for reference only.https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/132881/1/Getting%20Starte...
Thanks & Regards,Dhruvit Vasavada