make file error in mcuxpresso ide

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

make file error in mcuxpresso ide

1,066件の閲覧回数
kavyav
Contributor I

The attatched image contains error ,plz share the solution to this

0 件の賞賛
返信
1 返信

1,041件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @kavyav,

I hope you are doing well.

From the image, It is seen that error is with the below statement
"make -r -j4 all" terminated with exit code 2. The build might be incomplete.

I have a few queries to ask.
->Which IMX board are you using?
->Have you made any changes to Makefile or are you using the default given SDK

I have shared a link to docs please refer to section 5.1 (Build an app using Linux host) for reference only.
https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/132881/1/Getting%20Starte...

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信