make: *** No rule to make target `lib_id3_parser_arm11_elinux_intermediates/export_includes'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

make: *** No rule to make target `lib_id3_parser_arm11_elinux_intermediates/export_includes'

跳至解决方案
5,236 次查看
xingruizhu
Contributor III

Dear supporter

 

when we set  HAVE_FSL_IMX_CODEC := true in the file external/fsl_vpu_omx/codec_env.mk ,

there is a build error. Please ref the attach log for more info.

 

- Platform info -

  • IMX6DL
  • Android 5.0.2

 

Import includes file: out/et1D_em101/target/product/partner/obj/SHARED_LIBRARIES/libaudiopolicymanagerdefault_intermediates/import_includes

Import includes file: out/et1D_em101/target/product/partner/obj/SHARED_LIBRARIES/libcameraservice_intermediates/import_includes

make: *** No rule to make target `out/et1D_em101/target/product/partner/obj/SHARED_LIBRARIES/lib_id3_parser_arm11_elinux_intermediates/export_includes', needed by `out/et1D_em101/target/product/partner/obj/SHARED_LIBRARIES/libmediaplayerservice_intermediates/import_includes'.  Stop.

make: *** Waiting for unfinished jobs....

Import includes file: out/et1D_em101/target/product/partner/obj/SHARED_LIBRARIES/libmedialogservice_intermediates/import_includes

 

 

#### make failed to build some targets (07:19 (mm:ss)) ####

Original Attachment has been moved to: build_android_2016-01-07_1726.log.zip

0 项奖励
回复
1 解答
2,903 次查看
xingruizhu
Contributor III

update:

After patch the omx player, those bugs is fixed.

- android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz

To apply android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz patches, carry out the following commands:
$ cp android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz ~/myandroid
$ cd ~/myandroid
$ tar xzvf android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz
After unpacking this package, the current build mode is “full”, which means omxplayer feature will be built into the Android
platform.
Use switch_build_to.sh to switch between “core” mode and “full” mode.
$ ./switch_build_to.sh (display current mode)
$ ./switch_build_to.sh mode (mode shall be "core" or "full")
$ ./clean_obj_before_building.sh (clean related binary in the out directory of previous
Android build)

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,903 次查看
xingruizhu
Contributor III

Dear supporter

Those configs conflict with each other.

1. frameworks/av/media/libmediaplayerservice/Android.mk

46 ifeq ($(HAVE_FSL_IMX_CODEC),true)

47 LOCAL_SHARED_LIBRARIES +=                       \

48     lib_omx_player_arm11_elinux \

49     lib_omx_osal_v2_arm11_elinux \

50     lib_omx_client_arm11_elinux \

51     lib_omx_utils_v2_arm11_elinux \

52     lib_omx_core_mgr_v2_arm11_elinux \

53     lib_omx_res_mgr_v2_arm11_elinux \

54     lib_id3_parser_arm11_elinux

55 endif

2. external/fsl_vpu_omx/utils/id3_parser/Android.mk

  1 ifeq ($(HAVE_FSL_IMX_CODEC),false)

  2

  3

  4 LOCAL_PATH:= $(call my-dir)

  5 include $(CLEAR_VARS)

  6

  7 LOCAL_SRC_FILES := \

  8     ID3.cpp

  9

10 LOCAL_CFLAGS += $(FSL_OMX_CFLAGS)

11 LOCAL_LDFLAGS += $(FSL_OMX_LDFLAGS)

12 LOCAL_C_INCLUDES += $(FSL_OMX_PATH)/../../external/icu/icu4c/source/common \

13 +--  5 lines: $(FSL_OMX_PATH)/../../external/icu/icu4c/source/i18n \---------------------------------------------------------

18

19 LOCAL_SHARED_LIBRARIES := libstagefright libstagefright_foundation libutils libc liblog libmedia lib_omx_osal_v2_arm11_elinux

20

21 LOCAL_PRELINK_MODULE := false

22 LOCAL_MODULE_TAGS := eng

23 LOCAL_MODULE:= lib_id3_parser_arm11_elinux

24

25 include $(BUILD_SHARED_LIBRARY)

26

27 endif

0 项奖励
回复
2,904 次查看
xingruizhu
Contributor III

update:

After patch the omx player, those bugs is fixed.

- android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz

To apply android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz patches, carry out the following commands:
$ cp android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz ~/myandroid
$ cd ~/myandroid
$ tar xzvf android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz
After unpacking this package, the current build mode is “full”, which means omxplayer feature will be built into the Android
platform.
Use switch_build_to.sh to switch between “core” mode and “full” mode.
$ ./switch_build_to.sh (display current mode)
$ ./switch_build_to.sh mode (mode shall be "core" or "full")
$ ./clean_obj_before_building.sh (clean related binary in the out directory of previous
Android build)

0 项奖励
回复
2,903 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello xingrui,

    Yes, you are right!

     you forgot to do patch of coder and decoder files! the steps are in android user's guide.

Regards,

Weidong

0 项奖励
回复
2,903 次查看
xingruizhu
Contributor III

Thank you.

0 项奖励
回复