lvds display fuzzy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lvds display fuzzy

Jump to solution
1,988 Views
liyu1
Contributor III

HI all:

         I am using a 1080P screen (LG), findings show that fuzzy, as shown below: Customers say the problem can be solved by exchanging lvds cable(P and M exchange), but they do not want to change from the hardware above, if you can modify the parameters by software。Use this set of parameters, most of the lvds screen display properly !

    

      "LDB-1080P60", 60, 1920, 1080, 6451,

       240,0,//148, 88,

      69, 0,

      30, 8,

       0,

     FB_VMODE_NONINTERLACED,

        FB_MODE_IS_DETAILED,},

   20140627_143055.jpg

            20140627_143112.jpg

Tags (2)
0 Kudos
Reply
1 Solution
1,634 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

This issue can be closed

View solution in original post

0 Kudos
Reply
2 Replies
1,635 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

This issue can be closed

0 Kudos
Reply
1,636 Views
Paul_Kuhn
NXP Employee
NXP Employee

Li yu, Can you add some more detail about which Freescale products you are using?  There is a lot of expertise in the community and the more detail you can provide the easier it is for the right experts to share their knowledge.  

0 Kudos
Reply