HI all:
I am using a 1080P screen (LG), findings show that fuzzy, as shown below: Customers say the problem can be solved by exchanging lvds cable(P and M exchange), but they do not want to change from the hardware above, if you can modify the parameters by software。Use this set of parameters, most of the lvds screen display properly !
"LDB-1080P60", 60, 1920, 1080, 6451,
240,0,//148, 88,
69, 0,
30, 8,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},