load u-boot to imx6q sabrelite ,but see no output in serial console

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

load u-boot to imx6q sabrelite ,but see no output in serial console

4,091 次查看
panpanli
Contributor II

I have both used mfgtool and imx_usb_loader to load u-boot.bin or u-boot.imx to imx6q sabrelite ,but neither works,since I can't see U-Boot launch  on the serial console,and I'm sure the serial console have been correctly setted ,and the boot mode switches have been setted to 00 – Fuses.

here is the output on the terminal of ubuntu 10.04 ,when I use imx_usb_loader to load  u-boot.imx to BD-SL-i.MX6:

pp@pp-desktop:~/imx_usb_loader$ sudo ./imx_usb u-boot.imx

No "_" environment variable

argc == 2, argv == 0xbfb912f4

base == 0x804fc20:./imx_usb

trailing slash == 0x804fc21:/imx_usb

conf_path == ./

config file <./imx_usb.conf>

No "_" environment variable

argc == 2, argv == 0xbfb912f4

base == 0x804fc20:./imx_usb

trailing slash == 0x804fc21:/imx_usb

conf_path == ./

config file <./mx6_usb_work.conf>

parse mx6_usb_work.conf

15a2:0054(mx6_qsb) bConfigurationValue =1

Interface 0 claimed

report 1, wrote 16 bytes, err=0

report 3, read 4 bytes, err=0

read=56 78 78 56

u-boot.imx 0 0 1 0 1 2

main dcd length 310

sub dcd length 30c

dcd_ptr=0x177ff02c

loading binary file(u-boot.imx) to 177ff000, skip=0, fsize=4ee44 type=aa

<<<323140, 323140 bytes>>>

jumping to 0x177ff000

does u-boot load to the board ?if so,why I can't see any output in the serial console?I am so confused,

and I also have used the mfgtool,here is the information in the mfgtool.log:

Panel A Start <CMD/> type="find" body="Recovery" file="" timeout="180" onError="" text="".

1 - Panel A Finished <CMD/> type="find" body="Recovery" file="" timeout="180" onError="" text="" SUCCESS code=0x0.

Panel A Start <CMD/> type="boot" body="Recovery" file="u-boot-mx6q-sabrelite.bin" timeout="10" onError="" text="Loading uboot.".

1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="u-boot-mx6q-sabrelite.bin" timeout="10" onError="" text="Loading uboot." SUCCESS code=0x0.

Panel A Start <CMD/> type="load" body="" file="uImage" timeout="10" onError="" text="Doing Kernel.".

1 - Panel A Finished <CMD/> type="load" body="" file="uImage" timeout="10" onError="" text="Doing Kernel." SUCCESS code=0x0.

Panel A Start <CMD/> type="load" body="" file="initramfs.cpio.gz.uboot" timeout="10" onError="" text="Doing Initramfs.".

1 - Panel A Finished <CMD/> type="load" body="" file="initramfs.cpio.gz.uboot" timeout="10" onError="" text="Doing Initramfs." SUCCESS code=0x0.

Panel A Start <CMD/> type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. ".

1 - Panel A Finished <CMD/> type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. " SUCCESS code=0x0.

Panel A Start <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="".

it seems the u-boot have been successfully load to the board,does it?but there is neither no output in the serial console, I'm a freshman learning linux,I am eager to get the BD-SL-i.MX6 up,but it seems so many problems there since I can't boot the board,please help me!

标签 (2)
0 项奖励
回复
10 回复数

2,965 次查看
tonyzheng
NXP Employee
NXP Employee

Hi,

As far as I know, Nitrogen6_Lite that you use is provided by Boundary Device, not the standard reference board of freescale.So, I'm sorry that I can't reproduce your error.

0 项奖励
回复

2,965 次查看
panpanli
Contributor II

thank you all the same!it seems the board has two name imx6q sabrelite and bd-sl...is`t it produced by fresscale and two other companies? and in fact i need to load ubuntu in the board,and install qt in ubuntu,and i have successfully installed ubuntu in the board,but i don't know how to install qt.is that just as simple as it in pc?can i just use ‘apt-get’ to install qt?

0 项奖励
回复

2,965 次查看
tonyzheng
NXP Employee
NXP Employee

About standard reference board of freescale, pls refer to http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=IMX6X_SERIES&uc=true&lang_cd=en

You can't install QT only using 'apt-get'. Before installing QT, you should be sure that you hardware supports framebuffer and then install some necessary underlying graphics library. pls refer to http://qt-project.org/doc/qt-5/linux.html

If you are satisfied with the answer, pls close this question and submit correct reply. Thank you.

Regards,

Tony

0 项奖励
回复

2,965 次查看
tonyzheng
NXP Employee
NXP Employee

Hi, panpan

Do you have setup your serial console correctly?

Generally, the setup is 115200,8,NONE,1.

yours,

Tony

0 项奖励
回复

2,965 次查看
panpanli
Contributor II

Hi,TonyI'm sure I have set up the serial console correctly,now I have no idea about why no output in the serial console,can you help me?

0 项奖励
回复

2,965 次查看
tonyzheng
NXP Employee
NXP Employee

Hi,
Can i know where your board boot from?SD/MMC, eMMC4.3, eMMC4.4, eMMC4.41, SATA?

0 项奖励
回复

2,965 次查看
panpanli
Contributor II

I 'm not sure,maybe SD/MMC?

0 项奖励
回复

2,965 次查看
tonyzheng
NXP Employee
NXP Employee

hi, I advise you to boot the board from SD/MMC and it is easy!

  • Step 1:

Get a u-boot.bin. You can compile it through LTIB or use the standard image provided by Freescale

  • Step 2:

Copy the U-Boot image to the SD/MMC card as follows:

$ sudo dd if=u-boot-mx6q-sabresd.bin of=/dev/sdb bs=512 seek=2 skip=2 conv=fsync

  • Step 3

Insert the SD/MMC card to SD slot and power on the board.Now, you can boot the board from SD/MMC.

you can refer to i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide


0 项奖励
回复

2,965 次查看
panpanli
Contributor II

I have tried this method ,but also failed,since a error came up

0 项奖励
回复

2,965 次查看
tonyzheng
NXP Employee
NXP Employee

Can you provide me more information?And I'm confuesd by you.

Are you sure your board is standard board of freescale? In my opinion, imx_usb_loader is not provided by freescale. It is a script file and you are unnecessary to use it. You can complie a u-boot image through LTIB or Yocto and copy it to SD card by yourself.

0 项奖励
回复