linux interrupt time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux interrupt time

3,041件の閲覧回数
2548903578
Contributor III

Hi,everyone

  When I use imx6sx to configure the interrupt, the external will trigger an interrupt every 20ms, but the interrupt is not entered immediately after the interrupt is triggered, and there will be a certain delay. This delay time is about 10us. The problem now is that it is okay if the delay is 10us each time, but I found that the time of each entry interrupt is not fixed, sometimes it is long and sometimes short. There will be a certain error in this way. Does anyone know how to solve this problem? We are expecting a reply.

0 件の賞賛
返信
5 返答(返信)

3,034件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

3,021件の閲覧回数
2548903578
Contributor III

Hi,igorpadykov

 Real-Time Edge Software does not support imx6sx platform, only imx6ull.

 
0 件の賞賛
返信

3,017件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

you can port it yourself using i.MX6ULL as example.

 

Best regards
igor

0 件の賞賛
返信

3,025件の閲覧回数
2548903578
Contributor III

Hi,igorpadykov 

Can rt patches make the interruption time stable? I tested it and found that it is not as good as not adding it. We are using pin input interrupt, does fiq support it? Our m4 can only open one interrupt, so no other interrupts can be used.

0 件の賞賛
返信

3,039件の閲覧回数
2548903578
Contributor III

I played the rt package and still the same situation.

0 件の賞賛
返信