[i.MX 8MN DDR4+MCIMX8M-AUD ] How to BT, eth0 enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.MX 8MN DDR4+MCIMX8M-AUD ] How to BT, eth0 enabled

435 Views
bryan_hong
Contributor V

Hello

I must use `fsl-image-af-littlekernel` to boot. If I use imx-image-multimedia, the boot failed at i.MX 8MN DDR4+MCIMX8M-AUD

But, I use `fsl-image-af-littlekernel`, these pulseaudio, pactl, pacmd commands not be included in rootfs.
and eth0 can not be up.
===
root@imx8mnddr4ab2:~# ifconfig eth0 up
[ 15.749082] fec 30be0000.ethernet eth0: Unable to connect to phy
ifconfig: SIOCSIFFLAGS: No such device
===

plz help me

thanks
Bryan

0 Kudos
1 Reply

428 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bryan

 

MCIMX8M-AUD board is supported in imx8mn-ddr4-evk.dts, one can find references to "audio_board"

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mn-evk.d...

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mn-ddr4-...

One can try Demo Image   i.MX 8M Nano EVK

and follow i.MX Audio Board Quick Start Guide

 

Best regards
igor

0 Kudos