Hi
Is there anyone familiar with gpio-imx-rpmsg.c driver, { .compatible = "fsl,imx-rpmsg-gpio" }? Perhaps not, since it is demonstrated only with i.MX7ULP, forums search doesn't give a lot of hits.
Is that driver supposed to work with libgpiod? I'm using kernel 5.4.x. gpioget shell command works, gpioset command works as well , gpiomon doesn't work:
# gpiomon gpiochip8 16
gpiomon: error waiting for events: No such device
As well sysfs doesn't list "edge" file here
# echo 272 > /sys/class/gpio/export
# ls /sys/class/gpio/gpio272
active_low device power suppliers value
consumers direction subsystem uevent
"edge" is present with i.MX7D native GPIO driver:
# echo 176 > /sys/class/gpio/export
root@rcserv:~# ls /sys/class/gpio/gpio176
active_low device edge subsystem uevent
consumers direction power suppliers value
Thanks
Edward