libgpiod with Linux gpio-imx-rpmsg.c driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

libgpiod with Linux gpio-imx-rpmsg.c driver

ソリューションへジャンプ
15,411件の閲覧回数
kef2
Senior Contributor V

Hi

Is there anyone familiar with gpio-imx-rpmsg.c driver, { .compatible = "fsl,imx-rpmsg-gpio" }? Perhaps not, since it is demonstrated only with i.MX7ULP, forums search doesn't give a lot of hits.

Is that driver supposed to work with libgpiod? I'm using kernel 5.4.x. gpioget shell command works, gpioset command works as well , gpiomon doesn't work:

# gpiomon gpiochip8 16
gpiomon: error waiting for events: No such device

As well sysfs doesn't list "edge" file here

# echo 272 > /sys/class/gpio/export
# ls /sys/class/gpio/gpio272
active_low  device      power       suppliers   value
consumers   direction   subsystem   uevent

 

"edge" is present with i.MX7D native GPIO driver:

# echo 176 > /sys/class/gpio/export
root@rcserv:~# ls /sys/class/gpio/gpio176
active_low  device      edge        subsystem   uevent
consumers   direction   power       suppliers   value

 

Thanks

Edward

0 件の賞賛
返信
1 解決策
15,395件の閲覧回数
kef2
Senior Contributor V

Hi Igor,

Indeed it doesn't matter, libgpiod or sysfs+poll(). RPMSG GPIO interrupts are documented ... but not implemented.

gpio-imx-rpmsg.c\gpio\drivers - linux-imx - i.MX Linux kernel (codeaurora.org)

Here's RPMSG callback with TBD:

 

static int gpio_rpmsg_cb(struct rpmsg_device *rpdev,
	void *data, int len, void *priv, u32 src)
{
	struct gpio_rpmsg_data *msg = (struct gpio_rpmsg_data *)data;

	if (msg->header.type == GPIO_RPMSG_REPLY) {
		gpio_rpmsg.reply_msg = msg;
		complete(&gpio_rpmsg.cmd_complete);
	} else if (msg->header.type == GPIO_RPMSG_NOTIFY) {
		gpio_rpmsg.notify_msg = msg;
		/* TBD for interrupt handler */
	} else
		dev_err(&gpio_rpmsg.rpdev->dev, "wrong command type!\n");

	return 0;
}

 

 Replacing TBD with generic_handle_irq() with right arguments make interrupts working. Both libgpiod and sysfs.

Perhaps complete version of driver is lost somewhere? It's of course good to write documentation first and then implement according to documentation. But, hm, I'd prefer both complete and working :-). As I understand iMX7ULP EVK doesn't use RPMSG GPIO interrupts, buttons are used by RPMSG keyboard driver.

 

Regards

Edward

元の投稿で解決策を見る

0 件の賞賛
返信
12 返答(返信)
15,396件の閲覧回数
kef2
Senior Contributor V

Hi Igor,

Indeed it doesn't matter, libgpiod or sysfs+poll(). RPMSG GPIO interrupts are documented ... but not implemented.

gpio-imx-rpmsg.c\gpio\drivers - linux-imx - i.MX Linux kernel (codeaurora.org)

Here's RPMSG callback with TBD:

 

static int gpio_rpmsg_cb(struct rpmsg_device *rpdev,
	void *data, int len, void *priv, u32 src)
{
	struct gpio_rpmsg_data *msg = (struct gpio_rpmsg_data *)data;

	if (msg->header.type == GPIO_RPMSG_REPLY) {
		gpio_rpmsg.reply_msg = msg;
		complete(&gpio_rpmsg.cmd_complete);
	} else if (msg->header.type == GPIO_RPMSG_NOTIFY) {
		gpio_rpmsg.notify_msg = msg;
		/* TBD for interrupt handler */
	} else
		dev_err(&gpio_rpmsg.rpdev->dev, "wrong command type!\n");

	return 0;
}

 

 Replacing TBD with generic_handle_irq() with right arguments make interrupts working. Both libgpiod and sysfs.

Perhaps complete version of driver is lost somewhere? It's of course good to write documentation first and then implement according to documentation. But, hm, I'd prefer both complete and working :-). As I understand iMX7ULP EVK doesn't use RPMSG GPIO interrupts, buttons are used by RPMSG keyboard driver.

 

Regards

Edward

0 件の賞賛
返信
15,304件の閲覧回数
nxf77080
NXP Employee
NXP Employee
"Replacing TBD with generic_handle_irq() with right arguments make interrupts working. Both libgpiod and sysfs." What are the right arguments if I may ask?
0 件の賞賛
返信
15,405件の閲覧回数
kef2
Senior Contributor V

to_irq is missing in the driver. With copy paste from other driver gpiomon seems waiting, proper RPMSG request seems being sent along with launch of gpiomon. Need to fix M4 part to make both parts working:

 

diff --git a/drivers/gpio/gpio-imx-rpmsg.c b/drivers/gpio/gpio-imx-rpmsg.c
index 418455f..4abbabb 100644
--- a/drivers/gpio/gpio-imx-rpmsg.c
+++ b/drivers/gpio/gpio-imx-rpmsg.c
@@ -310,6 +310,13 @@ static void imx_rpmsg_mask_irq(struct irq_data *d)
 	/* No need to implement the callback */
 }
 
+static int imx_rpmsg_gpio_to_irq(struct gpio_chip *gc, unsigned offset)
+{
+	struct imx_rpmsg_gpio_port *port = gpiochip_get_data(gc);
+
+	return irq_find_mapping(port->domain, offset);
+}
+
 static struct irq_chip imx_rpmsg_irq_chip = {
 	.irq_mask = imx_rpmsg_mask_irq,
 	.irq_unmask = imx_rpmsg_unmask_irq,
@@ -337,6 +344,7 @@ static int imx_rpmsg_gpio_probe(struct platform_device *pdev)
 	gc = &port->gc;
 	gc->of_node = np;
 	gc->parent = dev;
+	gc->to_irq = imx_rpmsg_gpio_to_irq;
 	gc->label = "imx-rpmsg-gpio";
 	gc->ngpio = IMX_RPMSG_GPIO_PER_PORT;
 	gc->base = of_alias_get_id(np, "gpio") * IMX_RPMSG_GPIO_PER_PORT;

 

Edit: as well "edge" file is present using GPIO sysfs.

Edward

0 件の賞賛
返信
15,399件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Edward

 

thanks for sharing patch, you are right by default gpio-imx-rpmsg driver is not supposed to work with libgpiod.

 

Best regards
igor

0 件の賞賛
返信
15,303件の閲覧回数
nxf77080
NXP Employee
NXP Employee
"Replacing TBD with generic_handle_irq() with right arguments make interrupts working. Both libgpiod and sysfs." What are the right arguments? Thanks in advance.
0 件の賞賛
返信
15,302件の閲覧回数
nxf77080
NXP Employee
NXP Employee
Oops...did not see the patch. Thanks so much!!!
0 件の賞賛
返信
15,293件の閲覧回数
kef2
Senior Contributor V

Hi, @nxf77080 

that patch above was only to fix missing interrupt `edge` file. See attached whole driver source file after additional mods. Interrupts and IO seem working well. Would be nice to get rid of static gpio_rpmsg struct, I've no time for it

Regards,

Edward

0 件の賞賛
返信
15,231件の閲覧回数
nxf77080
NXP Employee
NXP Employee
Hi kef2, Where is the corresponding M4 FreeRTOS application? Thanks in advance. Best Regards, Rob
0 件の賞賛
返信
15,221件の閲覧回数
kef2
Senior Contributor V

As a NXP employee you should know much better than me where to get examples for corresponding Cortex-M code. It was quite hard to get answer: get MCUXpresso SDK for i.MX7ULP.

Regards

Edward

0 件の賞賛
返信
15,215件の閲覧回数
nxf77080
NXP Employee
NXP Employee

Yep, have the SDK.  Thought maybe you had made mods to the M4 side.

Thanks

0 件の賞賛
返信
15,156件の閲覧回数
kef2
Senior Contributor V

Of course I had to shave tons of codes unsuitable for i.MX7D code, I can't share it.

GPIO interrupts already are implemented in SDK. Cortex-M GPIO interrupt handler includes SRTM_IoService_NotifyInputEvent() call. This call is used to signal GPIO interrupt over RPMSG. This works well with edge sensitive interrupts. Level sensitive interrupts should limit reporting rate, else RPMSG queue may overflow. It should be implemented on Cortex-M. 

Edward

0 件の賞賛
返信
15,147件の閲覧回数
nxf77080
NXP Employee
NXP Employee

Thanks.  I figured some rate limiting would have to be employed on the M4 side for level sensitive interrupts.

Best Regards,

Rob

0 件の賞賛
返信