latest Linux on Sabrelite ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

latest Linux on Sabrelite ?

2,158件の閲覧回数
kmoran
Contributor I

I'm assuming that this is totally unsupported, but has anyone tried booting the latest Linux kernel(s) on the Sabrelite board ?  I have both a Sabrelite and a SabreSD and Linux-3.9-rc2 boots fine on the SabreSD but appears to hang on the Sabrelite.  I'm thinking that there maybe driver or configuration issues with the Sabrelite builds that I'm unfamiliar with, but I thought I would ask around before breaking out the JTAG debugger.

Thanks,

-Kevin

ラベル(3)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,808件の閲覧回数
LeonardoSandova
Specialist I

Yocto should be able to build a correct uImage. In case you are compiling manually, the BD git repo has the url for the android and non-android repos.

https://github.com/boundarydevices/linux-imx6

Leo

0 件の賞賛
返信

1,808件の閲覧回数
kmoran
Contributor I

Thanks Leo, but I was looking for something more along the lines of the mainline linux kernel.  I have all the various BD git trees.

Best regards,

-Kevin

0 件の賞賛
返信