gpu-viv-bin-mx6q buildroot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gpu-viv-bin-mx6q buildroot

ソリューションへジャンプ
5,883件の閲覧回数
richc128
Contributor III

Is there a way to integrate the gpu-viv-bin-mx6q package in buildroot?

I can only extract these binaries over the rootfilesystem. But, they seem to be built with a compilar that I can't seem to find. I did try the one included with ltib with no luck.

Are there sources for these binaries?

http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/

ラベル(2)
0 件の賞賛
返信
1 解決策
3,511件の閲覧回数
andre_silva
NXP Employee
NXP Employee

Hi Richard,

the integration only can be done using the package you got in this link, unfortunately the source code is not provided.

To have access to the source codes you need to contact freescale via customer support service and ask for the source. In this case, you will need to do some agreements and accept the terms and conditions to have access to it.

regards,

Andre

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,512件の閲覧回数
andre_silva
NXP Employee
NXP Employee

Hi Richard,

the integration only can be done using the package you got in this link, unfortunately the source code is not provided.

To have access to the source codes you need to contact freescale via customer support service and ask for the source. In this case, you will need to do some agreements and accept the terms and conditions to have access to it.

regards,

Andre

0 件の賞賛
返信
3,511件の閲覧回数
richc128
Contributor III

Don’t suppose you have contact info?

0 件の賞賛
返信
3,511件の閲覧回数
andre_silva
NXP Employee
NXP Employee

Yes it was, but it has to be done via Customer support.

0 件の賞賛
返信
3,511件の閲覧回数
richc128
Contributor III

Thanks. I’ve submitted a ticket.

0 件の賞賛
返信
3,511件の閲覧回数
andre_silva
NXP Employee
NXP Employee

thank you.

0 件の賞賛
返信