kit kat release for saberesd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kit kat release for saberesd

5,781 Views
oslreddy
Contributor II

HI group

can any body tell me when is the expected date of releasing kitkat for saberesd (i.MX6Q)

Thanks

Labels (4)
9 Replies

4,844 Views
ZBL
Contributor I

I want to know which version is the "Android KK4.4.2_1.0.0 GA " based on ?  android4.4.2r1 or android4.4.2r2 ?

Thanks.

0 Kudos
Reply

4,844 Views
m_c
Senior Contributor I

Copy from Android_User's_Guide.pdf of android_kk4.4.2_1.0.0-ga_docs

~/bin/repo init -u https://android.googlesource.com/platform/manifest -b android-4.4.2_r1

0 Kudos
Reply

4,844 Views
m_c
Senior Contributor I

Android 4.4.2 1.0.0  has released at Freescale website at 7/14. However, it is broken link. Maybe it takes time to upload.

i.MX 6Quad Processors – Quad Core|Freescale

https://www.freescale.com/webapp/Download?colCode=JB44_100_ANDROID_SOURCE_BSP&appType=license&locati...

4,844 Views
m_c
Senior Contributor I
0 Kudos
Reply

4,844 Views
SergioSolis
NXP Employee
NXP Employee

Hello,

I'm sorry, there is still no date of release for KitKat

0 Kudos
Reply

4,844 Views
MaxChou
Contributor III

dear   Sir.

do you have any update for android 4.4 release schedule?

thank you

max


0 Kudos
Reply

4,843 Views
tonyzheng
NXP Employee
NXP Employee

Hello,

Android KK4.4.2_1.0.0 GA will be released in following months, and now it is under alpha test! Many FAEs will get the android version in July.

0 Kudos
Reply

4,844 Views
chayouncheul01
Contributor I

Hello.

I can't find "/device/wfd-proprietary/" described in "i.MX_Android_Wi-Fi_Display_Sink_API_Introduction.pdf".


"i.MX_Android_Extended_Wi-Fi_Display_Sink_Release_Notes.pdf" document describes as follow :

   --> "They are only available after applied android_kk4.4.2_1.0.0_wfdsink_source.tar.gz software package"


Where can i download "android_kk4.4.2_1.0.0_wfdsink_source.tar.gz" ?

0 Kudos
Reply

4,844 Views
tonyzheng
NXP Employee
NXP Employee

Hi, cha

wfd-proprietary is Freescale Extended Features with freescale-propritary and now is a paid package. In order to obtain this package, you can contact FAE or Market.

0 Kudos
Reply