kernel 6.4.8 infinite rootwait

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kernel 6.4.8 infinite rootwait

2,839 Views
Cécile
Contributor I

Hello, I'm updating the Linux kernel of an i.MX6Q-based SBC to kernel 6.4.8 (Debian distribution).
However, I'm encountering an infinite rootwait.
The SD card is not mounted in the /dev folder (I checked from the initramfs console).
I'm also seeing a lot of 'not linking [...] might never become dev' errors starting from 1.755544s. The errors are as follows:

[ 1.736203][ T1] /soc/bus@2000000/gpc@20dc000: Relaxing link with /soc/bus@2000000/clock-controller@20c4000
[ 1.746272][ T1] /soc/bus@2000000/gpc@20dc000: Relaxing link with /soc/interrupt-controller@a01000
[ 1.755544][ T1] /soc: Relaxing link with /soc/bus@2000000/gpc@20dc000

I think it's a DTS/DTB problem, but I haven't found anything specific yet...

Please find below/in attachement :
- the boot logs
- kernel .config file
- dts, dtsi files

Thank you for your time,

Cécile Janin

0 Kudos
Reply
2 Replies

2,723 Views
Cécile
Contributor I

Hello,
To be sure:
Can I compile a kernel for imx6 only with the code downloaded from kernel.org ? Or should I add non-free binaries?

0 Kudos
Reply

2,736 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can check the 6.1v kernel BSP version since this is the latest official for MX6Q:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Regards

 

0 Kudos
Reply