issue with uboot include/config.h

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

issue with uboot include/config.h

跳至解决方案
4,693 次查看
wangtsungli
Contributor IV

Hi Community,

I'm working on i.MX6 sabresd Quad and build Android 6.0.

While I build u-boot I follow below commands.

  1. make distclean
  2. make mx6Qandoid_defconfig
  3. make -j8 2>&1 | tee uboot_err.log

While the build process I get the error here.

In file included from board/freescale/FM10A/FM10A.c:12:0:
./arch/arm/include/asm/arch/mx6-pins.h:46:2: error: #error "Please select cpu"
#error "Please select cpu"
^
AS arch/arm/lib/vectors.o
CC arch/arm/imx-common/iomux-v3.o
In file included from board/freescale/FM10A/FM10A.c:38:0:
./arch/arm/include/asm/arch/mx6-ddr.h:19:2: error: #error "Please select cpu"
#error "Please select cpu"
^
AS arch/arm/lib/crt0.o
board/freescale/FM10A/FM10A.c:98:2: error: 'MX6_PAD_CSI0_DAT10__UART1_TX_DATA' undeclared here (not in a function)
MX6_PAD_CSI0_DAT10__UART1_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),

so I trace the code I find out that my include/config.h did not defined some parameter.

Below is my config.h

/* Automatically generated - do not edit */
#define CONFIG_BOARDDIR board/freescale/FM10A
#include <config_defaults.h>
#include <config_uncmd_spl.h>
#include <configs/FM10A.h>
#include <asm/config.h>
#include <config_fallbacks.h>

What I miss are below define.

#define CONFIG_IMX_CONFIG board/freescale/FM10A/mx6q_4x_mt41j128.cfg
#define CONFIG_MX6Q 1
#define CONFIG_ANDROID_SUPPORT 1

I had check board/freescal/FM10A/MAINTAINER and Kconfig, two files is as below.

MAINTAINER

MX6SABRESD BOARD
M: Fabio Estevam <[email protected]>
S: Maintained
F: board/freescale/FM10A/
F: include/configs/FM10A.h
F: configs/mx6DLandroid_defconfig
F: configs/mx6Qandroid_defconfig

Kconfig

if TARGET_FM10A

config SYS_BOARD
default "FM10A"

config SYS_VENDOR
default "freescale"

config SYS_SOC
default "mx6"

config SYS_CONFIG_NAME
default "FM10A"

endif

Also I had check arch/arm/Kconfig, I did add a new target like below.

config TARGET_FM10A
bool "Support FM10A"
select CPU_V7
select SUPPORT_SPL

source "board/freescale/FM10A/Kconfig"

Also I had check /configs/mx6Qandroid_defconfig, below is what I defined.

ONFIG_SYS_EXTRA_OPTIONS="IMX_CONFIG=board/freescale/FM10A/mx6q_1G.cfg,MX6Q,SYS_USE_SPINOR,ANDROID_SUPPORT"
CONFIG_ARM=y
CONFIG_TARGET_FM10A=y
CONFIG_SYS_MALLOC_F=y
CONFIG_SYS_MALLOC_F_LEN=0x400
CONFIG_DM=y
CONFIG_DM_THERMAL=y

标签 (5)
0 项奖励
回复
1 解答
4,089 次查看
wangtsungli
Contributor IV

I had found solution.

I need to modify device/fsl/FX100/Boardconfig.mk

And change TARGET_BOOTLOADER_CONFIG parameter to imx6q:mx6Qandroid_defconfig imx6dl:mx6DLandroid_defconfig.

Then it solve my problem!

在原帖中查看解决方案

1 回复
4,090 次查看
wangtsungli
Contributor IV

I had found solution.

I need to modify device/fsl/FX100/Boardconfig.mk

And change TARGET_BOOTLOADER_CONFIG parameter to imx6q:mx6Qandroid_defconfig imx6dl:mx6DLandroid_defconfig.

Then it solve my problem!