Hi,
How can I download and boot firmware from QSPI flash of MIMXRT1050 EVK board?
I tried IAR, Keil and Mfgtool2 to download firmware to QSPI flash, but all of them failed.
Anyone know if this is possible via jlink?
Hi tom,
please take a look to MIMXRT1050 EVK Board Hardware User’s Guide
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Carios,
yes, i did over two weeks ago, it doesn't due to HW or EVK board, i think there isn't IAR flashloader for this QSPI flash.
Hi tom,
IAR does not provide a mechanism to flash QSPI, you may download the Flashloader for i.MXRT1050 which supports QSPI NOR Flash here:
www.nxp.com/imxrt1050 > Software & Tools > Flashloader i.MX-RT1050
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
it's hopeful, are you sure it supports QSPI NOR Flash? i go through the files, it seems that just only hyperflash files, do you know which one is for QSPI NOR flash?
Hello Tom, I also noticed this. Did you ever resolve how to program QSPI Flash with the FlashLoader/MfgTool?
Thanks.
yes, after changing .bd file, Mfgtool can download firmware to QSPI flash, but you know, it can't debug, just run the program.
Hello Tom, thanks for the reply. Would you mind posting your modified script? I'm sure it would be helpful as more people begin using this part.
I think I've got it. I took program_flexspinor_image_hyperflash.bd and changed the line 'load 0xc0233007 > 0x2000;' to 'load 0xc0100003 > 0x2000;' and I am now able to program a demo app into QSPI. See section 8.2.2.1 of the FlashLoader Reference Manual.
Thanks.
by the way, if i populate another QSPI flash rather than the default one, of cause, they are pin to pin, something of the flashloader i need to change?