issue related to processor selection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

issue related to processor selection

1,253 Views
samarora
Contributor I

Hi, i want to use imx6DL processor in my board and i don't need DDR3 RAM so i am thinking of using asynchronous SRAM. I want to know does 64 bit writes allowed to external SRAM or i have to break iit into two 32 bit writes? My application strongly required 64 bit writes.

0 Kudos
Reply
1 Reply

1,218 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sam

asynchronous SRAM can be connected to EIM bus i.MX6DL, it has

max. 32 bit width, as shown on Table 40. EIM Internal Module Multiplexing

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply