issue related to processor selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

issue related to processor selection

1,257件の閲覧回数
samarora
Contributor I

Hi, i want to use imx6DL processor in my board and i don't need DDR3 RAM so i am thinking of using asynchronous SRAM. I want to know does 64 bit writes allowed to external SRAM or i have to break iit into two 32 bit writes? My application strongly required 64 bit writes.

0 件の賞賛
返信
1 返信

1,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sam

asynchronous SRAM can be connected to EIM bus i.MX6DL, it has

max. 32 bit width, as shown on Table 40. EIM Internal Module Multiplexing

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信