is this ok for android base ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

is this ok for android base ?

跳至解决方案
1,943 次查看
chenw
Contributor II

wei@wei-VirtualBox:~/work/android/imx-p9.0.0_2.3.0$ source imx_android_setup.sh Start fetching the source for android build
Setting REL_PACKAGE_DIR to /home/wei/work/android/imx-p9.0.0_2.3.0
repo: warning: Python 2 is no longer supported; Please upgrade to Python 3.6+.
repo: warning: Python 2 is no longer supported; Please upgrade to Python 3.6+.
Fetching projects:  28% (193/688) platform/packages/providers/UserDictionaryProvFetching projects:  31% (214/688) platform/hardware/qcom/sdm845/thermal
Fetching projects: 100% (688/688), done.
Checking out projects:  42% (289/688) platform/external/python/google-auth-httplChecking out projects:  50% (344/688) platform/external/subsampling-scale-image-Checking out projects:  77% (530/688) platform/packages/apps/SafetyRegulatoryInfChecking out projects:  80% (551/688) platform/packages/providers/ApplicationsPrChecking out projects:  86% (592/688) platform/prebuilts/gcc/linux-x86/arm/arm-lChecking out projects: 100% (688/688), done.
repo sync has finished successfully.
Android source is ready for the build
wei@wei-VirtualBox:~/work/android/imx-p9.0.0_2.3.0/android_build$

标签 (1)
0 项奖励
回复
1 解答
1,864 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, it's OK, you can follow our user guide to build the android BSP.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,865 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, it's OK, you can follow our user guide to build the android BSP.

0 项奖励
回复
1,864 次查看
chenw
Contributor II

TKS

0 项奖励
回复