is this ok for android base ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is this ok for android base ?

ソリューションへジャンプ
1,932件の閲覧回数
chenw
Contributor II

wei@wei-VirtualBox:~/work/android/imx-p9.0.0_2.3.0$ source imx_android_setup.sh Start fetching the source for android build
Setting REL_PACKAGE_DIR to /home/wei/work/android/imx-p9.0.0_2.3.0
repo: warning: Python 2 is no longer supported; Please upgrade to Python 3.6+.
repo: warning: Python 2 is no longer supported; Please upgrade to Python 3.6+.
Fetching projects:  28% (193/688) platform/packages/providers/UserDictionaryProvFetching projects:  31% (214/688) platform/hardware/qcom/sdm845/thermal
Fetching projects: 100% (688/688), done.
Checking out projects:  42% (289/688) platform/external/python/google-auth-httplChecking out projects:  50% (344/688) platform/external/subsampling-scale-image-Checking out projects:  77% (530/688) platform/packages/apps/SafetyRegulatoryInfChecking out projects:  80% (551/688) platform/packages/providers/ApplicationsPrChecking out projects:  86% (592/688) platform/prebuilts/gcc/linux-x86/arm/arm-lChecking out projects: 100% (688/688), done.
repo sync has finished successfully.
Android source is ready for the build
wei@wei-VirtualBox:~/work/android/imx-p9.0.0_2.3.0/android_build$

ラベル(1)
0 件の賞賛
返信
1 解決策
1,853件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, it's OK, you can follow our user guide to build the android BSP.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,854件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, it's OK, you can follow our user guide to build the android BSP.

0 件の賞賛
返信
1,853件の閲覧回数
chenw
Contributor II

TKS

0 件の賞賛
返信