is there a simple disc image I can use to boot the mcimx6ul?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is there a simple disc image I can use to boot the mcimx6ul?

1,358件の閲覧回数
jacobmunoz
Contributor I

I'm new to this device, and just want a simple, vanilla, ready-to-write-to-sd-card ISO/IMG file to boot a mcimx6ul.

I've spent  hours trying to fight with this "build" system... and it's not working - and too much guessing, I get this error at some point and gave up.

~/Documents/mx6/fsl-release-bsp/out$ bitbake fsl-image-gui

ERROR:  OE-core's config sanity checker detected a potential misconfiguration.

    Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).

    Following is the list of potential problems / advisories:

    Failed to create a file with a long name in TMPDIR. Please use a filesystem that does not unreasonably limit filename length.

Failed to create a file with a long name in SSTATE_DIR. Please use a filesystem that does not unreasonably limit filename length.

If someone can give me a clue what to do to get this build system working?  Or if anyone out there has a working disc image I can just copy - it doesn't need to do jack squat but boot and show visual evidence that it boots.

0 件の賞賛
返信
1 返信

1,038件の閲覧回数
saurabh206
Senior Contributor III

Hi Jacob,

You can download pre-built image from

i.MX 6 Series Software and Development Tool|NXP

For yocto following link will be useful.

i.MX Yocto Project: Frequently Asked Questions

Thanks

Saurabh

0 件の賞賛
返信