install QT5 on Linaro-Ubuntu

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

install QT5 on Linaro-Ubuntu

跳至解决方案
3,752 次查看
hjpark71
Contributor III

In order to install QT5 on my Linaro-Ubuntu running on IMX6, I run this command on 5.6 and 5.7..


./configure -opengl es2 -device linux-imx6-g++ -device-option CROSS_COMPILE=/opt/gcc-linaro-4.9-2015.02-3-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf- -sysroot ~/rootfs -prefix /usr/local/qt5 -opensource -confirm-license -optimized-qmake -reduce-exports -release -make libs -prefix /usr/local/qt5 -v

but, I always face so many errors.  it is one of them but all errors are related with includes

/opt/gcc-linaro-4.9-2015.02-3-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=hard --sysroot=/home/smart/rootfs -O2 -Wall -W -fPIC -I. -I../../../mkspecs/devices/linux-imx6-g++ -o opengles2.o opengles2.cpp
opengles2.cpp:37:25: fatal error: GLES2/gl2.h: No such file or directory
#include <GLES2/gl2.h>
^
compilation terminated.
make: *** [opengles2.o] Error 1
OpenGL ES 2.0 disabled.
The OpenGL ES 2.0 functionality test failed!
You might need to modify the include and library search paths by editing
QMAKE_INCDIR_OPENGL_ES2, QMAKE_LIBDIR_OPENGL_ES2 and QMAKE_LIBS_OPENGL_ES2 in
/home/smart/Qt/5.6/Src/qtbase/mkspecs/devices/linux-imx6-g++.

I don't understand why QT5 is so stupid as he doesn't find inc files what are already in his own Src tree.

Do you have any complete guy for installing QT5 into Linaro-Ubuntu? thanks..

标签 (2)
1 解答
2,388 次查看
b36401
NXP Employee
NXP Employee

Here is a document regarding to QT5 installation:

https://community.nxp.com/docs/DOC-96390

Have a great day,                                                                                                                                                                  

Victor                                                                                                                                                                             

                                                                                                                                                                                   

-----------------------------------------------------------------------------------------------------------------------                                                            

Note: If this post answers your question, please click the Correct Answer button. Thank you!                                                                                       

-----------------------------------------------------------------------------------------------------------------------                                                            

在原帖中查看解决方案

2 回复数
2,389 次查看
b36401
NXP Employee
NXP Employee

Here is a document regarding to QT5 installation:

https://community.nxp.com/docs/DOC-96390

Have a great day,                                                                                                                                                                  

Victor                                                                                                                                                                             

                                                                                                                                                                                   

-----------------------------------------------------------------------------------------------------------------------                                                            

Note: If this post answers your question, please click the Correct Answer button. Thank you!                                                                                       

-----------------------------------------------------------------------------------------------------------------------                                                            

2,388 次查看
hjpark71
Contributor III

Hi Victor,

Many thanks for your great help...

HJ

0 项奖励
回复