in linux when i do make error is accured

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

in linux when i do make error is accured

1,173 次查看
pooja_todakar
Contributor I

hi i m pooja,

when i did  "make iw_rainbowg18_defconfig" i m getting  this below error.how to resolve that

In function `imx6sl_enter_wait':
cpuidle-imx6sl.c:(.text+0x64): undefined reference to `psci_ops'

0 项奖励
回复
1 回复

1,124 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pooja

probably non-nxp linux was used, please try linux from official source.codeaurora.org/external/imx/linux-imx/

repository
linux-imx - i.MX Linux kernel 

Documentation

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复