imxrt1060 : SocketException when debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxrt1060 : SocketException when debug

ソリューションへジャンプ
2,108件の閲覧回数
morganRo
Contributor II

Hi everyone, 

I am stuck with my imx1060 evk board, when i try too debug every sdk example the probe failed.

Error pop up appears with SocketException : connection reset

SocketError.PNGSocketError.PNG

 

I try to reconnected/disconneted board, uninstall/install driver, uninstall/install MCUExpresso without any success.

imxrt1060.PNGimxrt1060.PNG

I also try on another PC and I can debug on it, so it only hapen on my PC.

One more think strange, I have also an imxrt1050 evk and it works fine until today, since this morning imxrt1050 doesn't work exactly like the 1060.

Thanks by advance

0 件の賞賛
返信
1 解決策
2,105件の閲覧回数
morganRo
Contributor II

I thinks I solved the problem,

Instead of uninstall/install driver in device manager, I uninstall device in printer device.

And for now it works.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,106件の閲覧回数
morganRo
Contributor II

I thinks I solved the problem,

Instead of uninstall/install driver in device manager, I uninstall device in printer device.

And for now it works.

0 件の賞賛
返信