imxg2dcompositor with imxv4l2src/imxv4l2videosrc err

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxg2dcompositor with imxv4l2src/imxv4l2videosrc err

Jump to solution
1,409 Views
adorable
Contributor III

We are now using imxg2dcompositor to compositing camera and videotestsrc.Using gstreamer1.0 as bellows.All videotestsrc is ok,but add imxv4l2videosrc or imxv4l2src is err as bellows.

Kernel 4.9.88  and using the latest gst-imx plugins...

gst-launch-1.0 \
imxg2dcompositor name=c background-color=0x223344 \
sink_0::xpos=0 sink_0::ypos=0 sink_0::width=400 sink_0::height=300 sink_0::fill_color=0x00000000 \
sink_1::xpos=400 sink_1::ypos=0 sink_1::width=400 sink_1::height=300 sink_1::fill_color=0x11111111 \
sink_2::xpos=200 sink_4::ypos=150 sink_4::width=400 sink_4::height=300 sink_4::fill_color=0x44444444 sink_4::alpha=0.5 ! \
queue2 ! video/x-raw, width=800, height=600 ! imxg2dvideosink \
videotestsrc pattern=2 ! queue2 ! c.sink_0 \
videotestsrc pattern=1 ! queue2 ! c.sink_1 \
imxv4l2videosrc device=/dev/video1 ! queue2 ! c.sink_2

----------------------------------------------------------------------------------------------------------------------------------------

errors:

(gst-launch-1.0:972): GLib-GObject-CRITICAL **: g_object_ref: assertion 'G_IS_OBJECT (object)' failed

(gst-launch-1.0:972): GStreamer-CRITICAL **: invalid unclassed object pointer for value type 'GstAllocator'
0:00:01.266664334 972 0x271d50 ERROR imxphysmembufferpool phys_mem_buffer_pool.c:110:gst_imx_phys_mem_buffer_pool_set_config:<imxphysmembufferpool8> pool configuration has NULL allocator set

(gst-launch-1.0:972): GStreamer-CRITICAL **: gst_object_unref: assertion '((GObject *) object)->ref_count > 0' failed
0:00:01.267518000 972 0x271d50 ERROR bufferpool gstbufferpool.c:555:gst_buffer_pool_set_active:<imxphysmembufferpool8> pool was not configured
0:00:01.267892667 972 0x271d50 ERROR imxblitter blitter.c:240:gst_imx_blitter_set_input_frame_internal:<imxg2dblitter1> error acquiring input frame buffer: unknown
0:00:01.268273334 972 0x271d50 ERROR imxvideocompositor compositor.c:873:gst_imx_video_compositor_aggregate_frames:<c> error while drawing composition frame

0 Kudos
Reply
1 Solution
1,397 Views
adorable
Contributor III

tht plugin imxg2dcompositor ony support as follows in my device imx6q:

imxv4l2videosrc device=/dev/video0 ! c.sink_0 \
imxv4l2videosrc device=/dev/video1 ! c.sink_1

or 

videotestsrc ! c.sink_0 \
videotestsrc ! c.sink_1

and videosrc to imxg2dcompositor should be directely,not support data filter between them.

View solution in original post

0 Kudos
Reply
1 Reply
1,398 Views
adorable
Contributor III

tht plugin imxg2dcompositor ony support as follows in my device imx6q:

imxv4l2videosrc device=/dev/video0 ! c.sink_0 \
imxv4l2videosrc device=/dev/video1 ! c.sink_1

or 

videotestsrc ! c.sink_0 \
videotestsrc ! c.sink_1

and videosrc to imxg2dcompositor should be directely,not support data filter between them.

0 Kudos
Reply