imx93 u-boot-spl.bin load to sram passthrough trace32 run error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93 u-boot-spl.bin load to sram passthrough trace32 run error

780 Views
juno
Contributor I

load u-boot-spl.bin to sram passthrought trace32.

when access trdc register

U-Boot SPL 2023.04-g0d202df47f (Oct 03 2024 - 11:40:25 +0800)
SOC: 0xa1009300
LC: 0x40010
PMIC: Over Drive Voltage Mode
"Synchronous Abort" handler, esr 0x96000010
elr: 000000002049bd58 lr : 000000002049bf4c
x 0: 0000000049010000 x 1: 0000000000028100
x 2: 0000000044460010 x 3: 0000000000000010
x 4: 0000000000000000 x 5: 0000000000000000
x 6: 00000000010a0400 x 7: 00000000204b2f18
x 8: 0000000020502378 x 9: 0000000000000080
x10: 0000000020501b30 x11: 00000000204abf48
x12: 00000000204b5ed8 x13: 00000000204b5ed8
x14: 0000000000000065 x15: 0000000000000109
x16: 00000000204a7578 x17: 0000000000000000
x18: 0000000020501bf0 x19: 000000000000000e
x20: 0000000020487000 x21: 000000004761bcda
x22: 0000000020487000 x23: 00000000204874e0
x24: 0000000044460044 x25: 000000000000f0f0
x26: 0000000044210028 x27: 0000000000000000
x28: 0000000000000000 x29: 0000000020501bd0

Code: 128002a0 17ffffe0 128001a0 17ffffde (b9400000)
Resetting CPU ...

resetting ...

 

0 Kudos
Reply
1 Reply

760 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

This could be a bad implementation of the bootloader or bad burn, so please try to burn again with the UUU or JTAG.

Regards

0 Kudos
Reply