imx93 cm33 flexio pwm disable output pin in the timer interrput

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93 cm33 flexio pwm disable output pin in the timer interrput

933 Views
lidafu
Contributor II

Hello,

I'm running an application on IMX93 CM33 core and I'm using FLEXIO as the PWM output.

The PWM signal is working good, but our application scenario requires PWM output stop at some certain conditions while re-enable.

Is it possible to enable/disable the PWM output while still keeping the FLEXIO timer running?

Tags (2)
0 Kudos
Reply
1 Reply

909 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer FlexIO PWM mode example code for i.MX93 via NXP Github.

You can set PWM working in idle status if duing application to disable PWM output.

PWM demo detailed info could check here

Wish it helps.

Mike

0 Kudos
Reply