imx93 UUU starts uboot but dont execute fastboot commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx93 UUU starts uboot but dont execute fastboot commands

ソリューションへジャンプ
1,017件の閲覧回数
spawn
Contributor III

Hello,

I'm trying to boot and flash an imx93 using uuu, but it's not working.

Uboot starts but then uuu  does not seem to run fastboot commands to flash.

Run built-in script:                                
 uuu_version 0.0.1                                  
                                                    
# @_image                  | bootloader             
                                                                                                         
SDPS: boot -f x-u-boot.bin                                                                                                                                    
FB: ucmd mmc dev 0                                                                                       
FB: flash mmc0boot0 x-u-boot.bin                    
FB: done                                            
                                                                                                         
                                                                                                         
Wait for Known USB Device Appear...                                                                      
New USB Device Attached at 3:41-E5EA7500DEF94036                                                         
3:41-E5EA7500DEF94036>Start Cmd:SDPS: boot -f x-u-boot.bin                                                                                                    
100%3:41-E5EA7500DEF94036>Okay (4.759s) 

 Do you know why ?

ps: once uboot is running, if I run 'fastboot usb 0' , then I can use uuu to run the fastboot commands that did not seem to run before.

0 件の賞賛
返信
1 解決策
1,010件の閲覧回数
spawn
Contributor III

I guess I have start fastboot automatically somehow.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,011件の閲覧回数
spawn
Contributor III

I guess I have start fastboot automatically somehow.

0 件の賞賛
返信