imx8qxp partitioning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8qxp partitioning

跳至解决方案
1,425 次查看
_angelo_
Contributor III

Hi all,

on imx8qxp i would need:

ADMA LPSPI peripheral - 0,1, 2,3  to M4

and

ADMA LPUART peripherals 0, 2 to A side

Both are using same edma (2) module so i am supposingm, using dma, the above partitioning is not possible.

Could someone confirm this ?

Thanks a lot

regards
angelo

 

0 项奖励
回复
1 解答
1,415 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

>Both are using same edma (2) module so i am supposingm, using dma, the above

>partitioning is not possible. Could someone confirm this ?

 

yes this is correct understanding.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,416 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

>Both are using same edma (2) module so i am supposingm, using dma, the above

>partitioning is not possible. Could someone confirm this ?

 

yes this is correct understanding.

 

Best regards
igor

0 项奖励
回复
1,407 次查看
_angelo_
Contributor III

Thanks !

0 项奖励
回复