imx8qxp partitioning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,108件の閲覧回数
_angelo_
Contributor III

Hi all,

on imx8qxp i would need:

ADMA LPSPI peripheral - 0,1, 2,3  to M4

and

ADMA LPUART peripherals 0, 2 to A side

Both are using same edma (2) module so i am supposingm, using dma, the above partitioning is not possible.

Could someone confirm this ?

Thanks a lot

regards
angelo

 

0 件の賞賛
返信
1 解決策
2,098件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

>Both are using same edma (2) module so i am supposingm, using dma, the above

>partitioning is not possible. Could someone confirm this ?

 

yes this is correct understanding.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,099件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

>Both are using same edma (2) module so i am supposingm, using dma, the above

>partitioning is not possible. Could someone confirm this ?

 

yes this is correct understanding.

 

Best regards
igor

0 件の賞賛
返信
2,090件の閲覧回数
_angelo_
Contributor III

Thanks !

0 件の賞賛
返信