imx8qxp partitioning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp partitioning

Jump to solution
1,600 Views
_angelo_
Contributor III

Hi all,

on imx8qxp i would need:

ADMA LPSPI peripheral - 0,1, 2,3  to M4

and

ADMA LPUART peripherals 0, 2 to A side

Both are using same edma (2) module so i am supposingm, using dma, the above partitioning is not possible.

Could someone confirm this ?

Thanks a lot

regards
angelo

 

0 Kudos
Reply
1 Solution
1,590 Views
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

>Both are using same edma (2) module so i am supposingm, using dma, the above

>partitioning is not possible. Could someone confirm this ?

 

yes this is correct understanding.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
1,591 Views
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

>Both are using same edma (2) module so i am supposingm, using dma, the above

>partitioning is not possible. Could someone confirm this ?

 

yes this is correct understanding.

 

Best regards
igor

0 Kudos
Reply
1,582 Views
_angelo_
Contributor III

Thanks !

0 Kudos
Reply