imx8qm virtualization for android 11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm virtualization for android 11

Jump to solution
1,127 Views
zfreeman2321
Contributor I

hi, 

As description in the doc <IMXVIRTUG> ,  the Yocto Project build images with Xen would work for Linux L4.14.98 and Android P9.0.

Is there sth upgrade for L5.4 and Android 11 for the virtualization solution ?

Thanks

0 Kudos
Reply
1 Solution
1,121 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello zfeeman2321,

 

XEN works on Android 11 and kernel 5.10.52v if you want the kernel 5.4.70v should be android 10.

 

Regards

View solution in original post

0 Kudos
Reply
1 Reply
1,122 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello zfeeman2321,

 

XEN works on Android 11 and kernel 5.10.52v if you want the kernel 5.4.70v should be android 10.

 

Regards

0 Kudos
Reply