MCIMX8QM-CPU first boot fail. No HDMI / no serial

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX8QM-CPU first boot fail. No HDMI / no serial

821件の閲覧回数
ArturMatkowski
Contributor I

Hi All.

I have just unboxed the device and assembled it according to provided manual (power suply, usb cables, provided SD card). I have also set a serial settings as described in manual. Actually both in device manager, and TeraTerm. Windows does show 4 USB Serial ports. (COM3 to COM6). 

When I insert provided SD card (with preinstalled image) I can see no output on HDMI, nor any prompt on TeraTerm.

I also tried a different image, also no effect. My boot pins are at 001100. 

Basicly I haven't even started working with that board, Meaby I'm making some newbie mistake, missing something.

0 件の賞賛
返信
1 返信

807件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share more details on how you flashed a different image and the BSP version?

I believe that when you tried flashing a different image it was the same result, no response from any of the terminal COMs, correct?

Also, please note that the default display enabled should be trough LVDS-to-HDMI daughter card, which can be connected to any of the following J2/J3/J7/J8

Best regards,
Aldo.

0 件の賞賛
返信