imx8qm standalone (kernel-dts-modules) build process withount imx-make.sh

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qm standalone (kernel-dts-modules) build process withount imx-make.sh

413件の閲覧回数
proxy13
Contributor I

hey i m trying to compile imx8qm kernel code for Android automotive platform.

when i was use imx-make.sh file i can compile all kernel source .but i want compile each side by one by

for example modules only or dts without using imx-make.sh .

seems imx8qm uses

arch/arm64/configs/gki_defconfig

also merge it
mek_8q/automotive_addition_car2_defconfig and configs/imx8q_car_gki.fragment

as understood.

after than how can i compile kernel like

make ARCH=arm64 CROSS_COMPILE=${AARCH64_GCC_CROSS_COMPILE} <...defconfig>

make ARCH=arm64 CROSS_COMPILE=${AARCH64_GCC_CROSS_COMPILE} dtbs

make ARCH=arm64 CROSS_COMPILE=${AARCH64_GCC_CROSS_COMPILE} modules

 

my system envs.

export AARCH64_GCC_CROSS_COMPILE=~/gcc-arm-9.2-2019.12-x86_64-aarch64-none-elf/bin/aarch64-none
-elf-
export CLANG_PATH=~/prebuilt-android-clang
export PATH=~/prebuilt-android-kernel-build-tools/linux-x86/bin:$PATH
export ARMGCC_DIR=~/gcc-arm-none-eabi-7-2018-q2-update

 

 

 

thank u for reply again.

ラベル(2)
0 件の賞賛
返信
0 返答(返信)