imx8mq+yocto+4.9.51_ga:USB3.0 issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq+yocto+4.9.51_ga:USB3.0 issue

2,739件の閲覧回数
传策薛
Contributor V

Hi,community:

   

Our company has customized a motherboard for imx8mq, running yocto system, there are two usb3.0 interfaces on the motherboard, which are connected by two usb3.0hosts on the cpu, respectively connected to two usb3.0 interface cameras. At the same time, two cameras are taken to take the image stream, and the operation is normal at the beginning. After a period of time, the following error is printed:
[ 1163.760957] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.763187] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.765412] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.767643] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.769866] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.772090] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.774313] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.776538] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.778765] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.780990] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.783216] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.785440] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.787663] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.789894] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.792118] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.794342] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.796564] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.798786] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.801017] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.803243] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.805466] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.807692] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1163.809914] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.812142] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[ 1163.814363] xhci-hcd xhci-hcd.0.auto: Ring expansion failed
[1164.500502] systemd-journald[1737]: /dev/kmsg buffer overrun, some messages lost.
[ 1164.514332] xhci-hcd xhci-hcd.0.auto: Ring expansion failed

What is the problem with this?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 传策 薛

RE: XHCI: Ring expansion failure — Linux USB 

please try latest Linux L4.14.78

linux-imx - i.MX Linux kernel 
Linux L4.14.78_1.0.0 Documentation
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,316件の閲覧回数
传策薛
Contributor V

Is Linux L4.14.78 a GA version?

pastedImage_1.png

0 件の賞賛
返信

2,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes it is GA, one can check:

i.MX Software | NXP 

Best regards
igor

0 件の賞賛
返信